SPRAD86A March 2023 – May 2024 AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM68A , AM69A
The AM6xA ISP (VPAC) consists of multiple functional blocks. Raw images are processed by these blocks one after another. The tuning tool allows tuning of the ISP blocks in independent groups, with each group containing one or more ISP blocks. The tuning groups are referred as plug-ins, as shown in the tuning tool menu Plug-ins:
In general, tune these plug-ins in the same order of ISP blocks when processing the raw image. Below is a recommended tuning order:
There is a slight difference in tuning RGB-only sensors and RGB-IR sensors:
After tuning each plug-in, a new set of XML files for VPAC configuration can be generated. These new XML files can replace those generated from the initial configuration to gradually improve the image quality.
In this application note, the OX05B1S sensor is used to illustrate the tuning of PCID, and the IMX219 sensor is used for illustrating the tuning of the rest plug-ins including black level, AWB, color correction, and so forth. More details about tuning are available in the plug-in guides from the Help menu of the tuning tool. Other versions of ISP tuning tool from TI 3rd parties follow roughly the same procedure.