SPRADG5 January 2024 DRA821U , DRA821U-Q1 , TDA4AL-Q1 , TDA4VH-Q1 , TDA4VL-Q1 , TDA4VM , TDA4VM-Q1
Normally, the default PINs configurations of MCU_UART0 and WKUP_UART0 serial ports are not suggested to be modified during the customers’ hardware design stage. The reason is that ROM code uses the default pin setting of MCU_UART0 when doing OSPI burning, and SYSFW uses the default pin setting in WUKP_UART0. However, due to PIN conflicts and other reasons, MAIN_UARTX is often changed to a new serial port. Moreover, in multi-core debugging, a separate MAIN_UARTX serial port is often required to be configured for the DSP/MAIN_R5F core for debugging purpose.