SWRA513C January   2020  – September 2020 CC3120 , CC3120MOD , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF

 

  1.   Trademarks
  2. 1Introduction
    1. 1.1 Terminology
  3. 2Overview
    1. 2.1 General Description
  4. 3Provisioning Configuration Modes
    1. 3.1 AP Provisioning
    2. 3.2 SmartConfig Provisioning
    3. 3.3 AP Plus SmartConfig Provisioning
    4. 3.4 AP Plus SmartConfig Plus External Configuration Provisioning
  5. 4Initiating the Provisioning Process
    1. 4.1 Host-Initiated Provisioning
    2. 4.2 Auto-Provisioning
    3. 4.3 Ending the Provisioning Process
  6. 5Profile Confirmation
    1. 5.1 Feedback
      1. 5.1.1 Local Feedback
      2. 5.1.2 External Feedback (Cloud)
    2. 5.2 Confirmation Fail
  7. 6External Configuration
  8. 7Host APIs
    1. 7.1 Provisioning Command
    2. 7.2 Provisioning Status Event
    3. 7.3 Provisioning Profile-Added Event
    4. 7.4 Reset Request Event
    5. 7.5 Blocking APIs During Provisioning
  9. 8Provisioning Use Examples
    1. 8.1 Successful SmartConfig Provisioning
    2. 8.2 Unsuccessful SmartConfig Provisioning
    3. 8.3 Successful SmartConfig Provisioning With AP Fallback
    4. 8.4 Successful AP Provisioning
    5. 8.5 Successful AP Provisioning With Cloud Confirmation
    6. 8.6 Using External Configuration Method: WAC
    7. 8.7 Successful SmartConfig Provisioning While External Configuration Enabled
  10. 9Provisioning HTTP/HTTPS Server APIs
  11.   Revision History

Auto-Provisioning

When the auto-provisioning connection policy is enabled, the provisioning process automatically starts in the following cases:

  • No saved profiles exist, and 2 seconds have passed since the device started, without receiving any command from the host.
  • The device is in STA role, the auto-start connection policy is enabled, the profile list is not empty, and the device was disconnected from the WLAN network for more than 2 minutes.

If the provisioning process is auto-started while in STA role, SC-only configuration mode is used. If the provisioning process is started while in AP role, APSC configuration mode is used. Whenever a provisioning process is auto-started, a proper event notifies the host.