SWRA536 February   2016 CC2520 , CC2520 , CC2530 , CC2530 , CC2530-RF4CE , CC2530-RF4CE , CC2533 , CC2533 , CC2540 , CC2540 , CC2541 , CC2541 , CC2640 , CC2640 , CC2640R2F , CC2640R2F , CC2640R2F-Q1 , CC2640R2F-Q1 , CC2640R2L , CC2640R2L , CC2650 , CC2650 , CC2650MODA , CC2650MODA

 

  1.   ETSI EN 300 328 RX Blocking Test for Bluetooth Low Energy
    1.     Trademarks
    2. 1 Introduction
    3. 2 ETSI EN 300 328 V2.1.1 Requirement
    4. 3 Test Setup
      1. 3.1 Test Equipment
      2. 3.2 R&S Waveform
      3. 3.3 Connection
      4. 3.4 TX Setup
      5. 3.5 RX Setup
    5. 4 Measurement Data
      1. 4.1 TX CW Blocker Setup
      2. 4.2 Low Channel Sensitivity (2402 MHz)
      3. 4.3 High Channel Sensitivity (2480 MHz)
      4. 4.4 BLE PER vs Blocking Requirement (ETSI EN 300 328 V2.1.1)
    6. 5 References

Low Channel Sensitivity (2402 MHz)

Table 3. BLE PEP vs PER at 2402 MHz

Level PEP Ok pkt PER[%]
-105.0 -82.29 150 0.00 %
-106.0 -83.29 148 1.33 %
-107.0 -84.29 145 3.33 %
-108.0 -85.29 127 15.33 %
-108.5 -85.79 110 26.67 %
-109.0 -86.29 97 35.33 %
-110.0 -87.29 38 74.67 %

Measured sensitivity at 2402 MHz was found to be -86.05 dBm Peak Envelope Power (PEP). Wanted signal should, according to the Receiver Blocking Parameters Receiver Category 2 Equipment table in ETSI EN 300 328 V2.1.1, be set 6 dB above the sensitivity limits. With a measured sensitivity at -86.05 dBm that will lead to that the level on the wanted signal should be -80.09 dBm PEP (level = -102.8 dBm).

Note that there is a loss in the test setup at almost 10dB (see Section 4.1) so actual RX sensitivity level is around 96dBm.