SWRA714A July 2021 – November 2023 CC1312PSIP , CC1312R , CC1312R7 , CC1314R10 , CC1352P , CC1352P7 , CC1352R
The wfantund provides a native IPv6 network interface to a connected TI Wi-SUN® FAN border router that is operating in NWP mode. The repository (public on TI GitHub) provides software to run on a Linux host with a Wi-SUN® FAN NWP connected over UART. wfantund also offers the possibility to visualize the network topology graphically with the use of a webapp as shown in Figure 5. This webapp is also part of the wfantund GitHub repository.
Reference cross compilation support is provided for the TI AM64x platform as well as the BeaglePlay board.