TIDT286 June 2022
The requested custom load transient was rebuilt with electronic load HP6060B, see Figure 3-10.
In Figure 3-11 the output voltage waveform has a deviation of about 1% with bandwidth setting of 10 kHz.
|
Ch1 ⇒ VOUT 50 mV / div (AC) 10-kHz bandwidth Ch2 ⇒ IOUT 1 A / div 20-MHz bandwidth 10 ms / div |
The waveforms in Figure 3-12 are the same waveforms as in Figure 3-11 only with a different time scale.
|
Ch1 ⇒ VOUT 50 mV / div (AC) 10-kHz bandwidth Ch2 ⇒ IOUT 1 A / div 20-MHz bandwidth 400 µs / div |