One of the important performance requirements in the RF Transmitter is to provide constant
power across frequency in the band being used. Multiple external and internal factors (to
the device) cause change in the output power across frequency. This phenomenon is referred
to as RF droop in this document. An overview of reasons causing the RF droop is given
below
- Capacitors or inductors in the path: The output path of a transmitter contains
multiple capacitors and inductors either for some design purpose or can occur as parasitic
components. Since the impedance of these components changes with frequency, the output
power changes across frequency.
- Matching Circuits: Matching circuits are designed to make the frequency response
as flat as possible by matching the device impedance to the characteristic impedance of
the transmission system. Still some amount of non-flat frequency response is seen due to
the insertion losses and reflected power. Such frequency variation becomes prominent for
wide band applications as designing matching circuits for wide band applications is quite
difficult.
- Power amplifier: In general, systems employ a power amplifier at the output of
transmitter and before the antenna as shown in Figure 2-1. This power amplifier also gives rise to a particular frequency response according to
the parameters.