SBAA666 February 2025 AMC0106M05 , AMC0106M25
A picture of the test setup is shown in Figure 4-1. The left side shows the overall setup with the top side view of the 3-phase GaN inverter. The right side shows the area on the bottom side of the PCB where the AMC0106M05 is placed.
In the following measurements phase notation U, V, W is used instead of the phase A, B, C notation used on the PCB design and schematic. For example, phase C on the schematic equals phase W in the measurement.