SCPA062 July 2021 TCA9517
To illustrate this effect in a real I2C transaction, Figure 3-4 shows a test setup of two devices communicating over the I2C bus with the TCA9517 included for level translation.
The controller side is connected to the A side of the TCA9517 and the target is connected to the B side of the TCA9517.
Figure 3-5 shows a screen capture of the SCL and SDA lines on both sides of the TCA9517. Looking at the region after the eighth clock pulse, a very short spike is visible on the SDA line of the controller.