SLAAE71 December 2022 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507
The power management unit (PMU) generates the regulated core supplies for the device and provides supervision of the external supply. It also contains a bandgap voltage reference used by the PMU and other analog peripherals.
See from Figure 2-2, the power management unit (PMU) can provides supervision of the external supply, which is a common function in low-power application. Besides, PD0, PD1 and analog peripherals can be dedicated controlled to realize different power levels.
There are two supply supervisor circuits available. First is the fixed power-on reset (POR) circuit to indicate that the external supply has reached sufficient for the device to run correctly. Second is the user-programmable brownout reset (BOR) circuit which ensures that the external supply is maintained at a sufficient voltage to support correct operation of the device, which can be configured to other three BOR levels after startup.