SLAAEB3 may 2023 MSPM0L1106 , MSPM0L1106
PRODUCTION DATA
Read Current uses the DirectCommand function to read the CC2 current value from 0x3A and return the value. The read back value is reported in mA unit.
Table 4-4 shows how to read the 16-bit current measurement from CC2. The current value in the following waveform is 0x00F, which convert a decimal value of 15 mA.
Command | Name | Unit | Type | Description |
---|---|---|---|---|
0x3A | CC2 Current | userA | I2 | 16-bit CC2 current |