SLAU723A October 2017 – October 2018 MSP432E401Y , MSP432E411Y
Hibernation Calendar Control (HIBCALCTL)
The Hibernate calendar is enabled by setting the CALEN bit in the HIBCALCTL register. If the BCD bit is set, the fields are reported in BCD format.
HIBCALCTL is shown in Figure 6-21 and described in Table 6-16.
Return to Summary Table.
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | |||||||
R-0x0 | |||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||
R-0x0 | |||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | |||||||
R-0x0 | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | CAL24 | RESERVED | CALEN | ||||
R-0x0 | R/W-0x0 | R-0x0 | R/W-0x0 | ||||