SLVAFG6A December 2022 – November 2023 TPS25762-Q1 , TPS25772-Q1
Term | Description |
---|---|
Blind Sink | A Sink not returning Sink Capabilities per system power requirement. |
Contract | An agreement on power level reached between a Source and Sink. |
FSP | Fair Share Power |
Good Sink | A Sink correctly returning Sink Capabilities per system power requirement. |
Negotiation | The PD process between a Sink and Source:
|
PD | USB Power Delivery |
Port Partner | A USB Type-C PD device or host that is connected to a TPS257xx-Q1 port. In the scope of this application note, Port Partner is used to indicate a Sink. |
PDO | Power Data Object. What is used to expose a Source's power capabilities or a Sink's power requirements. |
Sink | The Port Partner consuming power from VBUS; most commonly a device. In this application note, Sink refers to devices connected to the TPS257xx-Q1. |
Sink Capabilities | A PD message reported by the Sink, which includes PDO to convey Sink's operational power requirements. Also referred to as Sink Cap. |
Source | The Port Partner supplying power over VBUS; most commonly a downstream facing port. In this application note, Source refers to the TPS257xx-Q1. |
Source Capabilities | A PD message reported by the Source, which includes PDO to convey Source's capabilities to provide power. Also referred to as Source Cap. |
SPM Engine | The TPS257xx-Q1's integrated subsystem responsible for the operational function of the Source Power Policy Management |