SLVAFG6A December 2022 – November 2023 TPS25762-Q1 , TPS25772-Q1
The TPS257xx-Q1 supports dynamic port power management scheme for VIN supply voltage fluctuations in case of Engine Start/Stop transition events. Through dynamic detection of the supply voltage input level, the SPM takes action to enter or exit the appropriate power level. Upon detection of low VIN below normal operating range, the SPM enters a lower power mode to protect the system from overheating. The SPM also filters a fluctuation or temporary glitch on VIN to prevent an abrupt loss of USB port power which in turn enhances the end user experience. Table 4-4 and Table 4-5 show the VIN threshold and timer parameters. All parameters are configured via the GUI except for VIN UVLO. Figure 4-5 depicts an example of how different power modes, as determined by the VIN threshold levels, work in conjunction with the deglitch filter and timers.
VIN Threshold Parameters | Description |
---|---|
VIN>EngOnVth | Full Power level entry threshold with EngineOnDeglitch filter(for example, Engine fully ON condition w/ Car Key Knob in ON position) |
VIN<EngOffNomVth | Full Power to Low power entry threshold with EngineOffDeglitch filter(i.e Car key knob in accessory position with nominal VIN accessory mode voltage level) |
VIN>EngineOnMinVth | No Power to Low Power entry threshold. This transition triggers entry into Low Power state immediately. If VIN remains above this threshold but below EngOnVth for EngineOffTimer duration, VBUS is disabled after the timer expiration. (for example, Car key knob in accessory position with lower VIN accessory mode voltage level) |
VIN<EngineOffMinVth | Any to No Power entry threshold after Engine Off Delay expiration. (for example, Car key knob in accessory position with lower VIN accessory mode voltage level) |
VIN<UVLO | Hardware VIN UVLO voltage level. The SPM Controller is disabled. |
Engine On/Off Timer Parameters | Description |
---|---|
EngOn Deglitch | Engine On Deglitch timer. Deglitch time to enter engine ON Full Power condition after VIN reaches EngOnVth. |
EngOff Deglitch | Engine Off Deglitch timer. Deglitch time to enter Low Power condition after VIN reaches EngOffNomVth. |
EngOnTimer(Grace Period) | Engine On timer (Grace Period Timer). Timeout value after Low Power entry from No Power. Once this timer expires and the VIN supply voltage is still below EngOnVth, VBUS is disabled. |
EngOffTimer(Grace Period) | Engine Off timer (Grace Period Timer). Timeout value after Low Power entry from Full Power. Once this timer expires, VBUS is disabled. |
Engine Off Delay | Engine Off Delay timer. Delay time to to enter No Power after VIN falls under EngOffMinVth. |
Figure 4-6 shows the GUI entry example in Advanced Configuration View.