SLVSAB4D June 2010 – January 2017 TPS61183
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
The TPS61183 provides a high-performance LED lighting solution for tablets, notebooks, monitors, and a variety of industrial designs. The device can drive 6 strings of 10 series LEDs in a compact and high efficient solution. The TPS61183 provides a gate driver to an external P channel MOSFET which can be turned off during device shutdown or fault condition.
For typical white-LED driver applications, use the parameters listed in Table 4.
DESIGN PARAMETER | EXAMPLE VALUE |
---|---|
Input voltage | 4.5 V to 24 V |
Output voltage | 38 V (maximum) |
LED string current | 30 mA (maximum) |
Switching frequency | 280 kHz to 1 MHz |
Because selection of the inductor affects power supply steady-state operation, transient behavior, and loop stability, the inductor is the most important component in switching-power-regulator design. There are three specifications most important to the performance of the inductor: inductor value, DC resistance, and saturation current. The TPS61183 is designed to work with inductor values between 10 µH and 47 µH. A 10-µH inductor is typically available in a smaller or lower profile package, while a 47-µH inductor may produce higher efficiency due to a slower switching frequency and/or lower inductor ripple. If the boost output current is limited by the overcurrent protection of the device, using a 10-µH inductor and the highest switching frequency maximizes controller output current capability.
Internal loop compensation for PWM control is optimized for the external component values, including typical tolerances, recommended in Table 5. Inductor values can have ±20% tolerance with no current bias. When the inductor current approaches saturation level, its inductance can decrease 20% to 35% from the 0-A value depending on how the inductor vendor defines saturation. In a boost regulator, the inductor DC current can be calculated with Equation 5.
where
The inductor current peak-to-peak ripple can be calculated with Equation 6.
where
Therefore, the peak current seen by the inductor is calculated with Equation 7.
Select an inductor with a saturation current over the calculated peak current. To calculate the worst-case inductor peak current, use the minimum input voltage, maximum output voltage, and maximum load current.
Regulator efficiency is dependent on the resistance of its high current path and switching losses associated with the PWM switch and power diode. Although the TPS61183 device has optimized the internal switch resistance, the overall efficiency is affected by the inductor DC resistance (DCR). Lower DCR improves efficiency. However, there is a trade-off between DCR and inductor footprint; furthermore, shielded inductors typically have higher DCR than unshielded ones. Table 5 lists the recommended inductors.
L (µH) | DCR (mΩ) | ISAT (A) | Size (L × W × H mm) | |
TOKO | ||||
A915AY – 4R7M | 4.7 | 38 | 1.87 | 5.2 × 5.2 × 3.0 |
A915AY – 100M | 10 | 75 | 1.24 | 5.2 × 5.2 × 3.0 |
TDK | ||||
SLF6028T – 4R7N1R6 | 4.7 | 38 | 1.87 | 5.2 × 5.2 × 3.0 |
SLF6028T – 4R7N1R6 | 10 | 75 | 1.24 | 5.2 × 5.2 × 3.0 |
The output capacitor is mainly selected to meet the requirement for output ripple and loop stability. This ripple voltage is related to the capacitance of the capacitor and its equivalent series resistance (ESR). Assuming a capacitor with zero ESR, the minimum capacitance needed for a given ripple can be calculated with Equation 8:
where
. The additional part of the ripple caused by ESR is calculated using:
Additionally, it is sometimes necessary to be aware of the output ripple voltage due to the ESR of the output capacitor where Vripple_ESR = IOUT × RESR. Due to its low ESR, Vripple_ESR can be neglected for ceramic capacitors, but must be considered if tantalum or electrolytic capacitors are used. The controller output voltage also ripples due to the load transient that occurs during PWM dimming. The TPS61183 adopts a patented technology to limit this type of output ripple even with the minimum recommended output capacitance. In a typical application, the output ripple is less than 250 mV during PWM dimming with a 4.7-µF output capacitor. However, the output ripple decreases with higher output capacitances.
The TPS61183 provides a gate driver to an external P channel MOSFET which can be turned off during device shutdown or fault condition. This MOSFET can provide a true shutdown function and also protect the battery from output short-circuit conditions. The source of the PMOS must be connected to the input, and a pullup resistor is required between the source and gate of the FET to keep the FET off during device shutdown. To turn on the isolation FET, the FAULT pin is pulled low and clamped at 8 V below the VBAT pin voltage. During device shutdown or fault condition, the isolation FET is turned off, and the input voltage is applied on the isolation MOSFET. During a short-circuit condition, the catch diode (D2 in the typical application circuit) is forward biased when the isolation FET is turned off. The drain of the isolation FET swings below ground. The voltage across the isolation FET can be momentarily greater than the input voltage. Therefore, select a 30-V PMOS for a 24-V maximum input. The on resistance of the FET has a large impact on power conversion efficiency because the FET carries the input voltage. Select a MOSFET with Rds(on) less than 100 mΩ to limit the power losses.