SPRACN0F October 2021 – March 2023 TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28384D , TMS320F28384S , TMS320F28386D , TMS320F28386S , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
There are a number of serial communication peripherals to choose from when designing a multi-device real-time control system. With processors needing to pass critical data between each other within very short periods of time, latency is a primary concern for the system designer.
Single data (D0) and clock (CLK) is minimum set of signals for FSI communications at 100Mbps with lowest signal count and isolation cost. #T5843526-290 shows that signal D1 is an optional data line used to achieve the full 200Mbps data rate of the FSI.
The FSI physical interface consists of three wires, a clock and two data signals, where one of the data signals is optional (see #T5843526-290). Data is transferred on both the rising and falling edge which permits a 50 MHz maximum FSI clock frequency to transfer data at 100 Mbps with two wires (CLK and D0) and 200 Mbps with three wires (CLK, D0, and D1). The high through-put along with defined data packets (frames) that contain limited header and footer allows data to be transferred between devices with very little latency. The FSI module consists of independent transmitter and receiver cores which allow for simultaneous full speed communications in both directions with no concept of a master or slave. A real-time system using FSI for distributed control is showcased in Distributed Multi-axis Servo Drive Over Fast Serial Interface (FSI) Reference Design.
Features that FSI offers over other commonly used communications peripherals include:
There are a number of system topologies which have components operating on both the “hot” (high voltage) and “cold” (low voltage) sides of the system that must communicate with each other. In this case digital isolators are used to bring data across an isolation barrier and the potential skew between signals that cross the isolation boundary can prove difficult to predict across many units of production. Even in systems without isolation, skew could be introduced by unequal signal trace lengths.
The delay line control feature at the receiver makes FSI well suited for this application as it can actively compensate for this skew (#T5843526-289) by adding delay to the individual FSI signals. See the Fast Serial Interface (FSI) Skew Compensation for more information on this differentiated feature. Also see the TMDSFSIADAPEVM for hardware evaluation of FSI with digital isolators.
Data is always transmitted and received on both the rising and falling edges of the FSI clock.
While only one data line is show in #T5843526-289 there is option of second data line in all FSI implementations