SPRUJ52C june 2022 – july 2023 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1
When enabled, the INTR_AGGR will provide a set of counters which will track how many outstanding messages have been observed for each ingress event index from the ingress Counted Global Event Transport Lane (ETL) interface. For each message received where the 'UpDn' flag is set, the corresponding counter will be incremented by value of the 'cnt' field of ingress message. Events where the 'UpDn' flag is cleared are ignored. The counter is made visible to software in the UDMA_INTA_COUNT_j register. When software has read the count, it can acknowledge that count has been seen and processed by writing back an integer value specifying the amount by which the counter should be decremented, and the counter will subtract that value from the current count (which may have updated since it was read). The count will saturate at a value of 0xFFFFFFFF. Writing a count 'ack' value higher than the one read is not supported and will produce non-deterministic results.
When a count transitions from zero to a non-zero value, a Global Up 'UpDn=1' event is sent out an egress ETL interface. When a count transitions from a non-zero value to zero, a down 'UpDn=0' event will be sent. The index of the Global event is mappable on a 'per-counter' basis, using the UDMA_INTA_MAP_j register. The event may be mapped such that it then re-enters INTR_AGGR's 'Event to Interrupt Bit Steering Block' to generate an interrupt to the host. The event routing is handled by an external event switch fabric. Note that writing a new egress event index via the UDMA_INTA_MAP_j register does not alter the stored event count for the ingress event register index.