Figure 12-352 shows the receive error handling schema for the MCASP, which can ONLY be implemented as part of the Rx polling sequence.
This register is for MCASP receive error handling: MCASP_RSTAT.
Note: - For more information about receive clock failure handling, see Section 12.5.2.3.16.6.3, Receive Clock Failure Check and Recovery.
- For more information about receive buffer overrun handling, see Section 12.5.2.3.16.2, Buffer Overrun Error - Receiver.
- For more information about DATA port Rx error handling, see Section 12.5.2.3.16.4, DATA Port Error - Receiver.
- For more information about unexpected Rx frame sync error handling, see Section 12.5.2.3.16.5, Unexpected Frame Sync Error.