SWCU185F january 2018 – march 2023 CC1312R , CC1352P , CC1352R , CC2642R , CC2642R-Q1 , CC2652P , CC2652PSIP , CC2652R , CC2652RB , CC2652RSIP , CC2662R-Q1
For compatibility with existing TI parts, the packet format given in Figure 26-9 can be used in most cases. This packet format is supported through the use of the commands CMD_PROP_TX and CMD_PROP_RX.
A more flexible packet format is also possible, as defined in Figure 26-10. This format is supported by the commands CMD_PROP_RX_ADV and CMD_PROP_TX_ADV. The format in Figure 26-9 is an example of this format.