SWCU185F january 2018 – march 2023 CC1312R , CC1352P , CC1352R , CC2642R , CC2642R-Q1 , CC2652P , CC2652PSIP , CC2652R , CC2652RB , CC2652RSIP , CC2662R-Q1
Mode 1 is intended for use when VIMS is in off mode or cache mode.
If VIMS is in cache mode, change the VIMS mode to off mode before powering down the VIMS domain. When the system is taken out of power down, you can set the VIMS mode back to cache mode, which invalidates (initializes) the cache memories (see Figure 9-6).
Mode 1 can also be used when the system is in GPRAM mode, but all data in the GPRAM is lost when the VIMS domain is set in power down.