For testing purposes, this reference design requires the following equipment:
- A power supply that is capable of supplying at least 2-A of load and up to 20-V.
- Current and Voltage Multimeters to measure the currents and voltages during the related tests.
- The TIDA-050055 board which is a printed circuit board (PCB) with all the devices in this design.
- Resistive load or electronic load that is capable at least 3-A.
- Thermal camera used to measure the thermal rise of the board during operation.
- Oscilloscope to capture voltages and a current.