Samples & Purchase Cart- |
- Contact Us
- |
- TI Worldwide: United States
- |
- my.TI Login
WEBENCH® Amplifier Designer
Op Amp Circuit Design Made Easy
Design op amp circuits in minutes with WEBENCH Amplifier Designer. Supported amplifier circuits include:
- Inverting Amplifiers
- AC-Coupled Inverting Amps
- Non-Inverting Amplifiers
- Integrators
- Low-Pass Filters
- High-Pass Filters
- Custom Filters
- and more!
Inverting AmplifierThe Inverting Amplifier multiplies the input voltage by the desired negative gain: Vout = -(Rf/Rg) x Vin Note that with a single positive supply voltage, the input voltage must be negative, so that a positive output can be developed. |
AC-Coupled Inverting AmplifierThe circuit multiplies the non-DC input voltage by the desired negative gain: Vout = [-(Rf/Rg) x Vin(p-p)] + Vbias Vbias is added to the noninverting input to bring that input voltage within normal amplifier operating range. It also provides an offset for the output, so it is within its operating range. Can also be used as a wide-bandwidth Bandpass Filter (20dB decade attenuation). For a narrow bandwidth filter, see the WEBENCH® Active Filter Designer |
Non-Inverting AmplifierThe Non-Inverting Amplifier multiplies the input voltage (Vin) by the desired positive gain, and subtracts a voltage proportional to the applied reference voltage: Vout = Vin x (1 + Rf/Rg) - Vref x (Rf/Rg) Note that if Vref = 0V, then the output voltage equation simplifies to: Vout = Vin x ( 1 + Rf/Rg) The feedback capacitor Cf rolls off the gain at frequencies above 1/2pi x RfCf, to attenuate high-frequency noise. |
||
Low-Pass FilterThe Sallen-Key lowpass biquad filter is a classic design. This implementation has low sensitivity to changes in component values over process, environment, and time. Using the 2nd-order Chebyshev approach gives a relatively steep rolloff near the cutoff frequency fc. For more information on this design, see application note OA-27. |
Low-Pass Filter 4th OrderThis 4th order lowpass filter uses a Sallen-Key topology for each of the two 2nd order sections. The user can select the desired filter approximation. Using the Chebyshev approach gives a relatively steep rolloff near the cutoff frequency fc, while a Bessel response produces a smoother step response. The Butterworth response has a nearly-flat passband, with a high-frequency rolloff of 20dB/decade for every pole (4 in this case). |
High-Pass FilterThe Sallen-Key highpass filter is a classic design. This implementation has low sensitivity to changes in component values over process, environment, and time. Using the 2nd-order Butterworth approach gives a straight-forward design with no peaking at the cutoff frequency fc. For more information on this design, see application note OA-29. |
||
Active FilterWEBENCH Active Filter Designer speeds the creation of advanced, highly customized filters. Filters may be specified by desired frequency response, or by a specific filter approximation and order. After the theoretical design is created, it is implemented using actual component values. The resulting filter can then be simulated. |
Sensor Analog Front End (AFE)For integrated LMP9xxxx Sensor AFE sensor circuit designs Sensor AFE products are highly integrated, (re)configurable sensor interface ICs with an easy-to-use hardware/software development platform. |
Sensor Path DesignFor discrete (sensor + amplifier + ADC) circuit designs The WEBENCH Sensor Designer tool provides a complete sensor to digital serial output solution, including sensor interface, excitation source, precision amplifier and filter, 8-bit through 16-bit ADCs, and a serialized output to connect to various back-end systems. |
||
IntegratorThe Integrator is used to calculate the integral of a signal. The output of the integrator is proportional to the area under the plot of voltage vs. time. For example, if the input signal is DC, then the output is a voltage ramp. Because integration involves a known start time and end time, a reset circuit must be included to establish the start time before each integration time period. The integration end time occurs when the measurement is read. |
||||