SPRS866G November 2012 ā October 2017 66AK2H06 , 66AK2H12 , 66AK2H14
PRODUCTION DATA.
Refer to the PDF data sheet for device specific package drawings
On the KeyStone II devices, the C66x CorePac, the EDMA3 transfer controllers and the system peripherals are interconnected through the TeraNets, which are nonblocking switch fabrics enabling fast and contention-free internal data movement. The TeraNets provide low-latency, concurrent data transfers between master peripherals and slave peripherals. The TeraNets also allow for seamless arbitration between the system masters when accessing system slaves.
The ARM CorePac is connected to the MSMC and the debug subsystem directly, and to other masters via the TeraNets. Through the MSMC, the ARM CorePacs can be interconnected to DDR3A and TeraNet 3_A, which allows the ARM CorePacs to access to the peripheral buses:
The C66x CorePacs, the ARM CorePacs, the EDMA3 traffic controllers, and the various system peripherals can be classified into two categories: masters and slaves.
Examples of masters include the EDMA3 traffic controllers and network coprocessor packet DMA.
Examples of slaves include the SPI, UART, and I2C.
The masters and slaves in the device communicate through the TeraNet (switch fabric). The device contains two types of switch fabric:
Some peripherals have both a data bus and a configuration bus interface, while others only have one type of interface. Furthermore, the bus interface width and speed varies from peripheral to peripheral.
Note that the data TeraNet also connects to the configuration TeraNet.
Figure 9-1, Figure 9-2, Figure 9-3, and Figure 9-4 show the connections between masters and slaves through various sections of the TeraNet.
Figure 9-1 TeraNet 3_A-1
Figure 9-2 TeraNet 3_A-2
Figure 9-3 TeraNet 3_C
Figure 9-4 TeraNet C66x to SDMA
Table 9-1 lists the master and slave end-point connections.
Intersecting cells may contain one of the following:
| MASTERS | SLAVES | |||||||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| AEMIF16 | BOOTROM_ARM | BOOTROM_C66X | COREPAC0_SDMA | COREPAC1_SDMA | COREPAC2_SDMA | COREPAC3_SDMA | COREPAC4_SDMA | COREPAC5_SDMA | COREPAC6_SDMA | COREPAC7_SDMA | DBG_STM | DDR3B | HYPERLINK0 | HYPERLINK1 | MSMC_SES | MSMC_SMS | PCIE | QM | SPI(0-2) | |
| 10GbE(1) | - | - | - | Y | Y | Y | Y | Y | Y | Y | Y | - | 10 | - | - | ses_2 | sms_2 | Y | Y | - |
| CorePac0_CFG | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| CorePac1_CFG | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| CorePac2_CFG | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| CorePac3_CFG | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| CorePac4_CFG | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| CorePac5_CFG | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| CorePac6_CFG | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| CorePac7_CFG | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| CPT_CFG | - | - | - | - | - | - | - | - | - | - | - | Y | - | - | - | - | - | - | - | - |
| CPT_DDR3A | - | - | - | - | - | - | - | - | - | - | - | Y | - | - | - | - | - | - | - | - |
| CPT_DDR3B | - | - | - | - | - | - | - | - | - | - | - | Y | - | - | - | - | - | - | - | - |
| CPT_INTC | - | - | - | - | - | - | - | - | - | - | - | Y | - | - | - | - | - | - | - | - |
| CPT_L2_(0-7) | - | - | - | - | - | - | - | - | - | - | - | Y | - | - | - | - | - | - | - | - |
| CPT_MSMC(0-7) | - | - | - | - | - | - | - | - | - | - | - | Y | - | - | - | - | - | - | - | - |
| CPT_QM_CFG1 | - | - | - | - | - | - | - | - | - | - | - | Y | - | - | - | - | - | - | - | - |
| CPT_QM_CFG2 | - | - | - | - | - | - | - | - | - | - | - | Y | - | - | - | - | - | - | - | - |
| CPT_QM_M | - | - | - | - | - | - | - | - | - | - | - | Y | - | - | - | - | - | - | - | - |
| CPT_SPI_ROM_EMIF16 | - | - | - | - | - | - | - | - | - | - | - | Y | - | - | - | - | - | - | - | - |
| CPT_TPCC(0_4)T | - | - | - | - | - | - | - | - | - | - | - | Y | - | - | - | - | - | - | - | - |
| CPT_TPCC(1_2_3)T | - | - | - | - | - | - | - | - | - | - | - | Y | - | - | - | - | - | - | - | - |
| DBG_DAP | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y |
| EDMA0_CC_TR | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| EDMA0_TC0_RD | 2,11 | 2,11 | 2,11 | Y | Y | Y | Y | Y | Y | Y | Y | - | Y | Y | Y | SES_0 | SMS_0 | Y | Y | 2,11 |
| EDMA0_TC0_WR | 2,11 | - | - | Y | Y | Y | Y | Y | Y | Y | Y | - | Y | Y | Y | SES_0 | SMS_0 | Y | Y | 2,11 |
| EDMA0_TC1_RD | 3,11 | 3,11 | 3,11 | Y | Y | Y | Y | Y | Y | Y | Y | - | Y | Y | Y | SES_1 | SMS_1 | Y | - | 3,11 |
| EDMA0_TC1_WR | 3,11 | - | - | Y | Y | Y | Y | Y | Y | Y | Y | - | Y | Y | Y | SES_1 | SMS_1 | Y | - | 3,11 |
| EDMA1_CC_TR | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| EDMA1_TC0_RD | 11 | 11 | 11 | Y | Y | Y | Y | Y | Y | Y | Y | - | 5 | Y | Y | SES_0 | SMS_0 | Y | Y | 11 |
| EDMA1_TC0_WR | 11 | - | - | Y | Y | Y | Y | Y | Y | Y | Y | Y | 5 | Y | Y | SES_0 | SMS_0 | Y | Y | 11 |
| EDMA1_TC1_RD | 11 | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | - | 6 | Y | Y | SES_1 | SMS_1 | Y | Y | 11 |
| EDMA1_TC1_WR | 11 | - | - | Y | Y | Y | Y | Y | Y | Y | Y | - | 6 | Y | Y | SES_1 | SMS_1 | Y | Y | 11 |
| EDMA1_TC2_RD | 11 | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | - | 7 | Y | Y | SES_1 | SMS_1 | Y | - | 11 |
| EDMA1_TC2_WR | 11 | - | - | Y | Y | Y | Y | Y | Y | Y | Y | - | 7 | Y | Y | SES_1 | SMS_1 | Y | - | 11 |
| EDMA1_TC3_RD | 11 | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | - | 8 | Y | Y | SES_1 | SMS_1 | Y | - | 11 |
| EDMA1_TC3_WR | 11 | - | - | Y | Y | Y | Y | Y | Y | Y | Y | Y | 8 | Y | Y | SES_1 | SMS_1 | Y | - | 11 |
| EDMA2_CC_TR | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| EDMA2_TC0_RD | 11 | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | - | 9 | Y | Y | SES_2 | SMS_2 | Y | Y | 11 |
| EDMA2_TC0_WR | 11 | - | - | Y | Y | Y | Y | Y | Y | Y | Y | Y | 9 | Y | Y | SES_2 | SMS_2 | Y | Y | 11 |
| EDMA2_TC1_RD | 11 | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | - | 10 | Y | Y | SES_2 | SMS_2 | Y | Y | 11 |
| EDMA2_TC1_WR | 11 | - | - | Y | Y | Y | Y | Y | Y | Y | Y | - | 10 | Y | Y | SES_2 | SMS_2 | Y | Y | 11 |
| EDMA2_TC2_RD | 11 | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | - | 5 | Y | Y | SES_0 | SMS_0 | Y | - | 11 |
| EDMA2_TC2_WR | 11 | - | - | Y | Y | Y | Y | Y | Y | Y | Y | Y | 5 | Y | Y | SES_0 | SMS_0 | Y | - | 11 |
| EDMA2_TC3_RD | 11 | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | - | 6 | Y | Y | SES_0 | SMS_0 | Y | - | 11 |
| EDMA2_TC3_WR | 11 | - | - | Y | Y | Y | Y | Y | Y | Y | Y | - | 6 | Y | Y | SES_0 | SMS_0 | Y | - | 11 |
| EDMA3_CC_TR | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| EDMA3_TC0_RD | 11 | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | - | 7 | Y | Y | SES_1 | SMS_1 | Y | Y | 11 |
| EDMA3_TC0_WR | 11 | - | - | Y | Y | Y | Y | Y | Y | Y | Y | Y | 7 | Y | Y | SES_1 | SMS_1 | Y | Y | 11 |
| EDMA3_TC1_RD | 11 | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | - | 8 | Y | Y | SES_1 | SMS_1 | Y | - | 11 |
| EDMA3_TC1_WR | 11 | - | - | Y | Y | Y | Y | Y | Y | Y | Y | - | 8 | Y | Y | SES_1 | SMS_1 | Y | - | 11 |
| EDMA4_CC_TR | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| EDMA4_TC0_RD | 2,11 | 2,11 | 2,11 | Y | Y | Y | Y | Y | Y | Y | Y | - | Y | Y | Y | SES_1 | SMS_1 | Y | Y | 2,11 |
| EDMA4_TC0_WR | 2,11 | - | - | Y | Y | Y | Y | Y | Y | Y | Y | - | Y | Y | Y | SES_1 | SMS_1 | Y | Y | 2,11 |
| EDMA4_TC1_RD | 3,11 | 3,11 | 3,11 | Y | Y | Y | Y | Y | Y | Y | Y | - | Y | Y | Y | SES_1 | SMS_1 | Y | - | 3,11 |
| EDMA4_TC1_WR | 3,11 | - | - | Y | Y | Y | Y | Y | Y | Y | Y | - | Y | Y | Y | SES_1 | SMS_1 | Y | - | 3,11 |
| HyperLink0_Master | 11 | 1,11 | 1,11 | Y | Y | Y | Y | Y | Y | Y | Y | - | Y | - | - | Y | Y | Y | Y | Y |
| HyperLink1_Master | 11 | 1,11 | 1,11 | Y | Y | Y | Y | Y | Y | Y | Y | - | Y | - | - | Y | Y | Y | Y | Y |
| MSMC_SYS | 11 | 11 | 11 | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | - | - | Y | Y | 11 |
| NETCP | - | - | - | Y | Y | Y | Y | Y | Y | Y | Y | - | 7 | - | - | SES_1 | SMS_1 | Y | Y | - |
| PCIE | 11 | - | - | Y | Y | Y | Y | Y | Y | Y | Y | Y | 10 | 10 | 10 | SES_2 | SMS_2 | - | Y | 11 |
| QM_Master1 | - | - | - | Y | Y | Y | Y | Y | Y | Y | Y | - | 5 | Y | Y | SES_0 | SMS_0 | - | Y | - |
| QM_Master2 | - | - | - | Y | Y | Y | Y | Y | Y | Y | Y | - | 8 | Y | Y | SES_1 | SMS_1 | - | Y | - |
| QM_SEC | - | - | - | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | SES_2 | SMS_2 | - | - | - |
| SRIO | 11 | - | - | Y | Y | Y | Y | Y | Y | Y | Y | Y | 9 | Y | Y | SES_2 | SMS_2 | - | Y | 11 |
| SRIO Packet DMA | 11 | - | - | Y | Y | Y | Y | Y | Y | Y | Y | - | 9 | - | - | SES_2 | SMS_2 | - | Y | - |
| USB | - | - | - | Y | Y | Y | Y | Y | Y | Y | Y | Y | 5 | Y | Y | SES_0 | SMS_0 | - | Y | - |
Figure 9-5, Figure 9-6, Figure 9-7, and Figure 9-8 show the connections between masters and slaves through various sections of the TeraNet.
Figure 9-5 TeraNet 3P_A
Figure 9-6 TeraNet 3P_B
Figure 9-7 TeraNet 6P_B
Figure 9-8 TeraNet 3P_Tracer
Table 9-2 and Table 9-3 list the master and slave end-point connections.
Intersecting cells may contain one of the following:
| MASTERS | SLAVES | ||||||||||||||||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| 10GBE_CFG | 10GBE_SERDES_CFG | ADTF(0-7)_CFG | ARM_CFG | BOOTCFG_CFG | CP_INTC_CFG | CPT_CFG_CFG | CPT_DDR3A_CFG | CPT_DDR3B_CFG | CPT_INTC(0-2)_CFG | CPT_L2_(0-7)_CFG | CPT_MSMC(0-7)_CFG | CPT_QM_CFG1_CFG | CPT_QM_CFG2_CFG | CPT_QM_M_CFG | CPT_SPI_ROM_EMIF16_CFG | DBG_CFG | DBG_TBR_SYS | DDR3A_PHY_CFG | DDR3B_PHY_CFG | EDMA0_CC_CFG | EDMA0_TC(0-1)_CFG | EDMA1_CC_CFG | EDMA1_TC(0-3)_CFG | EDMA2_CC_CFG | EDMA2_TC(0-3)_CFG | EDMA3_CC_CFG | EDMA3_TC(0-1)_CFG | EDMA4_CC_CFG | |
| 10GbE(1) | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| CorePac0_CFG | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y |
| CorePac1_CFG | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y |
| CorePac2_CFG | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y |
| CorePac3_CFG | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y |
| CorePac4_CFG | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y |
| CorePac5_CFG | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y |
| CorePac6_CFG | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y |
| CorePac7_CFG | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y |
| DBG_DAP | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y |
| EDMA0_CC_TR | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | Y | - | - | - | - | - | - | - |
| EDMA0_TC0_RD | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 12 | - | - | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 |
| EDMA0_TC0_WR | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 |
| EDMA0_TC1_RD | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 12 | - | - | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 |
| EDMA0_TC1_WR | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 |
| EDMA1_CC_TR | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | Y | - | - | - | - | - |
| EDMA1_TC0_RD | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 |
| EDMA1_TC0_WR | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | - | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 |
| EDMA1_TC1_RD | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 |
| EDMA1_TC1_WR | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 |
| EDMA1_TC2_RD | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 |
| EDMA1_TC2_WR | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 |
| EDMA1_TC3_RD | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 |
| EDMA1_TC3_WR | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | - | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 |
| EDMA2_CC_TR | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | Y | - | - | - |
| EDMA2_TC0_RD | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 |
| EDMA2_TC0_WR | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | - | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 |
| EDMA2_TC1_RD | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 |
| EDMA2_TC1_WR | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 |
| EDMA2_TC2_RD | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 |
| EDMA2_TC2_WR | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | - | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 |
| EDMA2_TC3_RD | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 |
| EDMA2_TC3_WR | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 |
| EDMA3_CC_TR | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| EDMA3_TC0_RD | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 |
| EDMA3_TC0_WR | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 |
| EDMA3_TC1_RD | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 14 | - | - | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 |
| EDMA3_TC1_WR | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 |
| EDMA4_CC_TR | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| EDMA4_TC0_RD | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 12 | - | - | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 |
| EDMA4_TC0_WR | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 |
| EDMA4_TC1_RD | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 12 | - | - | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 |
| EDMA4_TC1_WR | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 |
| HyperLink0_Master | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | - | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 |
| HyperLink1_Master | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | - | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 |
| MSMC_SYS | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y |
| NETCP | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| PCIE | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 |
| QM_Master1 | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 12 | - | 12 | - | 12 | - | 12 | - | 12 |
| QM_Master2 | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 12 | - | 12 | - | 12 | - | 12 | - | 12 |
| QM_SEC | 12 | - | - | 12 | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| SRIO | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 |
| SRIO Packet DMA | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| USB | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 12 | - | - | - | - | - | - | - | - | - | - | - |
| MASTERS | SLAVES | ||||||||||||||||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| EDMA4_TC(0-1)_CFG | GIC_CFG | GPIO_CFG | HYPERLINK0_SERDES_CFG | HYPERLINK1_SERDES_CFG | I2C(0-2)_CFG | MPU(0-14)_CFG | NETCP_CFG | NETCP_SERDES_CFG | PCIE_SERDES_CFG | PLL_CTL_CFG | PSC_CFG | QM_CFG1 | QM_CFG2 | SRIO_CFG | SRIO_SERDES_CFG | TBR_SYS_ARM | TETB0_CFG | TETB1_CFG | TETB2_CFG | TETB3_CFG | TETB4_CFG | TETB5_CFG | TETB6_CFG | TETB7_CFG | TIMER(0-19)_CFG | UART(0-1)_CFG | USB_MMR_CFG | USB_PHY_CFG | |
| 10GbE | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| CorePac0_CFG | Y | - | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y |
| CorePac1_CFG | Y | - | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y |
| CorePac2_CFG | Y | - | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y |
| CorePac3_CFG | Y | - | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y |
| CorePac4_CFG | Y | - | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y |
| CorePac5_CFG | Y | - | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y |
| CorePac6_CFG | Y | - | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y |
| CorePac7_CFG | Y | - | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y |
| DBG_DAP | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y |
| EDMA0_CC_TR | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| EDMA0_TC0_RD | 12 | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 12 | 12 | - | - | - | - | - | - |
| EDMA0_TC0_WR | 12 | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| EDMA0_TC1_RD | 12 | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 12 | 12 | - | - | - | - | - | - |
| EDMA0_TC1_WR | 12 | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| EDMA1_CC_TR | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| EDMA1_TC0_RD | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | - | - | - | - | 12 | 12 | - | - | 12 | 12 | 12 | 12 |
| EDMA1_TC0_WR | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | - | - | - | - | - | - | - | - | 12 | 12 | 12 | 12 |
| EDMA1_TC1_RD | 13 | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 13 | 13 | - | - | - | - | 13 | - | - | - | - | - |
| EDMA1_TC1_WR | 13 | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| EDMA1_TC2_RD | 14 | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 14 | 14 | - | - | - | 14 | - | - | - | - |
| EDMA1_TC2_WR | 14 | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| EDMA1_TC3_RD | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | - | - | - | - | 12 | 12 | - | - | 12 | 12 | 12 | 12 |
| EDMA1_TC3_WR | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | - | - | - | - | - | - | - | - | 12 | 12 | 12 | 12 |
| EDMA2_CC_TR | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| EDMA2_TC0_RD | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | - | - | - | - | Y | Y | - | - | 12 | 12 | 12 | 12 |
| EDMA2_TC0_WR | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | - | - | - | - | - | - | - | - | 12 | 12 | 12 | 12 |
| EDMA2_TC1_RD | 13 | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 13 | 13 | - | - | - | - | 13 | - | - | - | - | - |
| EDMA2_TC1_WR | 13 | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| EDMA2_TC2_RD | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | - | - | - | - | 12 | 12 | - | - | 12 | 12 | 12 | 12 |
| EDMA2_TC2_WR | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | - | - | - | - | - | - | - | - | 12 | 12 | 12 | 12 |
| EDMA2_TC3_RD | 14 | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 14 | 14 | - | - | - | 14 | - | - | - | - |
| EDMA2_TC3_WR | 14 | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| EDMA3_CC_TR | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| EDMA3_TC0_RD | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 |
| EDMA3_TC0_WR | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | 13 | - | - | - | - | - | - | - | - | 13 | 13 | 13 | 13 |
| EDMA3_TC1_RD | 14 | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | - | - | - | - |
| EDMA3_TC1_WR | 14 | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| EDMA4_CC_TR | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| EDMA4_TC0_RD | 12 | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 12 | - | - | - | - | 12 | 12 | - | - | - | - | - | - |
| EDMA4_TC0_WR | 12 | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 12 | - | - | - | - | - | - | - | - | - | - | - | - |
| EDMA4_TC1_RD | 12 | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 12 | - | - | - | - | 12 | 12 | - | - | - | - | - | - |
| EDMA4_TC1_WR | 12 | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 12 | - | - | - | - | - | - | - | - | - | - | - | - |
| HyperLink0_Master | 12 | - | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | - | - | - | - | - | - | - | - | 12 | 12 | 12 | 12 |
| HyperLink1_Master | 12 | - | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | - | - | - | - | - | - | - | - | 12 | 12 | 12 | 12 |
| MSMC_SYS | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y |
| NETCP | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| PCIE | 12 | - | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 |
| QM_Master1 | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| QM_Master2 | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| QM_SEC | - | - | - | - | - | - | - | 12 | - | - | - | - | - | - | - | - | 12 | - | - | - | - | - | - | - | - | - | - | 12 | - |
| SRIO | 14 | - | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 | 14 |
| SRIO Packet DMA | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - |
| USB | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | - | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | 12 | - | - | - | - |
The priority level of all master peripheral traffic is defined at the TeraNet boundary. User-programmable priority registers allow software configuration of the data traffic through the TeraNet. Note that a lower number means higher priority — PRI = 000b = urgent, PRI = 111b = low.
All other masters provide their priority directly and do not need a default priority setting. Examples include the C66x CorePacs, whose priorities are set through software in the UMC control registers. All the Packet DMA-based peripherals also have internal registers to define the priority level of their initiated transactions.
The Packet DMA secondary port is one master port that does not have priority allocation register inside the Multicore Navigator. The priority level for transaction from this master port is described by the QM_PRIORITY bit field in the CHIP_MISC_CTL0 register shown in Section 10.2.3.24.
For all other modules, see the respective User's Guides listed in Section 12.3 for programmable priority registers.