SBAS751B October 2017 – October 2018 ADS122C04
PRODUCTION DATA.
Up to 16 ADS122C04 devices can be connected to a single I2C bus by using different address pin configurations for each device. Use the address pins, A0 and A1, to set the ADS122C04 to one of 16 different I2C addresses. Figure 69 shows an example with three ADS122C04 devices on the same I2C bus. One set of pullup resistors is required per bus line. If needed, decrease the pullup resistor values to compensate for the additional bus capacitance presented by multiple devices and increased line length.
Figure 69. Connecting Multiple ADS122C04 Devices on the Same I2C Bus