SNLS472A January   2014  – June 2017 DS110DF1610

PRODUCTION DATA.  

  1. 1Features
  2. 2Description
  3. 3Revision History
  4. 4Pin Configuration and Functions
  5. 5Specifications
    1. 5.1 Absolute Maximum Ratings (DS110DF1610)
    2. 5.2 Recommended Operating Conditions
    3. 5.3 Thermal Characteristics
    4. 5.4 Electrical Characteristics
  6. 6Detailed Description
    1. 6.1 Overview
    2. 6.2 Functional Block Diagrams
    3. 6.3 Feature Description
      1. 6.3.1 Device Data Path Operation
        1. 6.3.1.1 AC-Coupled Receiver With Signal Detect
        2. 6.3.1.2 CTLE
        3. 6.3.1.3 Cross Point Switch
        4. 6.3.1.4 DFE With VGA
        5. 6.3.1.5 Clock and Data Recovery
        6. 6.3.1.6 Reference Clock
        7. 6.3.1.7 Differential Driver With FIR Filter
          1. 6.3.1.7.1 Setting the Output VOD
          2. 6.3.1.7.2 Output Driver Polarity Inversion
          3. 6.3.1.7.3 Driver Output Rise/Fall Time
      2. 6.3.2 Debug Features
        1. 6.3.2.1 Pattern Generator
        2. 6.3.2.2 Pattern Checker
        3. 6.3.2.3 Eye Opening Monitor
        4. 6.3.2.4 Interrupt Signals
      3. 6.3.3 Other Features
        1. 6.3.3.1 Lock Sequencer
    4. 6.4 Device Functional Modes
      1. 6.4.1 SMBus Slave Mode
        1. 6.4.1.1 SDA and SDC
        2. 6.4.1.2 Address Line
        3. 6.4.1.3 Device Configuration in SMBus Slave Mode
    5. 6.5 Programming
      1. 6.5.1 Bit Fields in the Register Set
      2. 6.5.2 Writing to and Reading from the Global/Shared/Channel Registers
    6. 6.6 Register Maps
      1. 6.6.1 Shared and Channel Registers
  7. 7Application and Implementation
    1. 7.1 Typical Applications
    2. 7.2 Initialization Setup
      1. 7.2.1 Data Rate Selection (Rate/Sub-Rate Table)
      2. 7.2.2 Data Rate Selection (Manual Programming)
  8. 8Power Supply Recommendations
    1. 8.1 Power Supply Filtering

Package Options

Mechanical Data (Package|Pins)
Thermal pad, mechanical data (Package|Pins)
Orderable Information

Application and Implementation

NOTE

Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.

Typical Applications

Figure 5 and Figure 6 show a typical application of the DS110Df1610. In these diagrams, the DS110DF1610 is configured for SMBus slave mode programming. Power is supplied to the device through a single 2.5V plane. The power supply filtering shown in these diagrams may need to be adjusted to accommodate additional system power noise. The SMBus and LVCMOS signals in this example use 2.5V logic. A differential reference clock for the digital block is applied to the device through 1µF AC-coupling capacitors. In this example, the high speed signals are connected to the device in groups of four to allow for the system designer to make use of the 4x4 cross point switches. Note that since the device contains AC-coupling capacitors on the high speed receiver inputs, the signals can be directly connected to the device. The transmitter outputs of this device should connect to AC-coupling capacitors placed near the receive inputs of the receiving ASIC.

DS110DF1610 TypicalConn.gif Figure 5. Typical Connection Diagram: Power and Control Pins
DS110DF1610 TypicalConn2.gif Figure 6. Typical Connection Diagram: High Speed Signals

Initialization Setup

The typical device initialization sequence for a DS110DF1610 includes the following:

  • Shared Register Configurations
    • Reference Clock Divider Setting (default is 125MHz)
    • Lock Sequencer Configuration (default is 8 channels allowed lock concurrently)
    :
  • Channel Register Configurations repeated for all desired channels:
    • CDR reset
    • Adapt Mode Configuration
    • Data rate selection
    • Output driver VOD and FIR configuration
    • Optional Continuous DFE adaption configuration
    • Optional Interrupt enable
    • Optional Reference clock loop through enable
    • Optional Cross point switch configuration
    • CDR reset release

Data Rate Selection (Rate/Sub-Rate Table)

The data rates for the DS110DF1610 must be known and programmed into each desired channel. The DS110DF1610 will only lock to programmed data rates and the programmed divider settings. For ease of use several common data rates have been preprogrammed into the DS110DF1610 along with the associated sub-rates for those various standards. These rate/sub-rate settings comprise the Rate/Sub-rate Table. Note that each channel operates independently, so different channels in the DS110DF1610 can operate at different data rates at the same time.

The Rate/Sub-rate table for the DS110DF1610 shown below includes all of the available preprogrammed data rates and associated divider groupings.

CHANNEL REGISTER 0x2F[7:4] SETTING STANDARD DATA RATES (Gbps) FIRST GROUP DIVIDER SETTINGS SECOND GROUP DIVIDER SETTINGS
0x0 Custom 1 5.0, 2.5 2, 4 2, 4
0xC Ethernet 1.25, 10.3125 8 1
0xD Fiber Channel (2.125, 4.25, 8.5), 10.51875 1, 2, 4 1
0xE SFF 8431 9.95328 1 1
0xF Custom 2 8.625, 4.3125 1, 2 1, 2

Data Rate Selection (Manual Programming)

The DS110DF1610 is capable of supporting any data rate within the specified range of 8.5 Gbps to 11.3 Gbps including the divide by 2, 4, and 8 sub-rates of this range. If it is desired to operate the DS110DF1610 at a data rate or data rate and sub-rate combination that is not available in the Rate/Sub-rate Table, then these desired data rates can be programmed into the device manually.

The following procedure describes how to calculate and manually program data rates into the DS110DF1610.

  1. Select a divider grouping from the Rate/Sub-rate Table and program that value to channel register 0x2F. When manually programming the data rate into the device, other rate/sub-rate values may be used to allow for different divider and group combinations. A list of all preprogrammed divider, group combinations is shown in the table below.
  2. CHANNEL REGISTER
    0x2F[7:4] SETTING
    FIRST GROUP DIVIDER SETTINGS SECOND GROUP DIVIDER SETTINGS
    0x0 2, 4 2, 4
    0x1 1 1
    0x2 1, 2, 4 1, 2, 4
    0x3 1, 2, 4 1, 2, 4
    0x4 1 1
    0x5 1 1
    0x6 1 1
    0x7 1, 2, 4 1, 2, 4
    0x8 1, 2, 4 1, 2, 4
    0x9 2, 4 2, 4
    0xA 1, 2, 4 1, 2, 4
    0xB 8 1
    0xC 8 1
    0xD 1, 2, 4 1
    0xE 1 1
    0xF 1, 2 1, 2
  3. Calculate the first group settings:
  4. PARAMETER VALUE/EQUATION COMMENT
    Reference Clock F0 = 25e6 Internally the reference clock always operates at 25 MHz
    Desired VCO Frequency F1 F1 is the frequency of the VC0 which is equal to the desired data rate. If the desired data rate uses dividers, be sure to multiply the data rate by the divide setting to get the correct VCO frequency
    Number of Reference Clocks N = 1024
    VCO Freq ÷ 32 F2 = F1 ÷ 32
    Counts of VCO Freq ÷ 32 required F3 = F2 x N ÷ F0
    Counts of VCO Freq ÷ 32 required rounded F4 Round F3 to the nearest integer value. Convert this value to binary. Program the upper 8 bits to ch register 0x61 and the lower 8 bits to ch register 0x60. Be sure to set channel register 0x61[7] to 1 to enable the override function for manual programming.
    PPM error due to rounding Err = 1e6 x (F4 – F3) ÷ F3
    Required PPM tolerance T Enter the desired PPM tolerance
    VCO Freq ÷ 32 +PPM tolerance F5 = (1+ T÷1e6) ÷ F2
    Rounded Counts of the VCO Freq ÷ 32 +PPM tolerance required F6 = F5 x N ÷ F0 Round F6 to the nearest integer value
    PPM Counts delta F7 = F6 – F3 Convert this value to binary. Program the most significant bit channel register 0x67[7] and the rest of the bits to channel register 0x64[7:4]
  5. Calculate the second group settings:
  6. PARAMETER VALUE/EQUATION COMMENT
    Reference Clock F0 = 25e6 Internally the reference clock always operates at 25 MHz
    Desired VCO Frequency F1 F1 is the frequency of the VC0 which is equal to the desired data rate. If the desired data rate uses dividers, be sure to multiply the data rate by the divide setting to get the correct VCO frequency
    Number of Reference Clocks N = 1024
    VCO Freq ÷ 32 F2 = F1 ÷ 32
    Counts of VCO Freq ÷ 32 required F3 = F2 x N ÷ F0
    Counts of VCO Freq ÷ 32 required rounded F4 Round F3 to the nearest integer value. Convert this value to binary. Program the upper 8 bits to ch register 0x63 and the lower 8 bits to ch register 0x62. Be sure to set channel register 0x63[7] to 1 to enable the override function for manual programming.
    PPM error due to rounding Err = 1e6 x (F4 – F3) ÷ F3
    Required PPM tolerance T Enter the desired PPM tolerance
    VCO Freq ÷ 32 +PPM tolerance F5 = (1+ T÷1e6) ÷ F2
    Rounded Counts of the VCO Freq ÷ 32 +PPM tolerance required F6 = F5 x N ÷ F0 Round F6 to the nearest integer value
    PPM Counts delta F7 = F6 – F3 Convert this value to binary. Program the most significant bit channel register 0x67[6] and the rest of the bits to channel register 0x64[3:0]

An example for setting group 0 and group 1 to 11.3 Gbps is shown in the table below.

CHANNEL REGISTER (HEX) VALUE
0x60 0x80
0x61 0xB8
0x62 0x80
0x63 0xB8
0x64 0xEE
0x67[7:6] 2'b00