SNOSCZ9 May 2016 FDC2112-Q1 , FDC2114-Q1 , FDC2212-Q1 , FDC2214-Q1
PRODUCTION DATA.
The FDC2112, FDC2114, FDC2212, and FDC2214 are high-resolution, multichannel capacitance-to-digital converters for implementing capacitive sensing solutions. In contrast to traditional switched-capacitance architectures, the FDC2112, FDC2114, FDC2212, and FDC2214 employ an L-C resonator, also known as L-C tank, as a sensor. The narrow-band architecture allows unprecedented EMI immunity and greatly reduced noise floor when compared to other capacitive sensing solutions.
Using this approach, a change in capacitance of the L-C tank can be observed as a shift in the resonant frequency. Using this principle, the FDC is a capacitance-to-digital converter (FDC) that measures the oscillation frequency of an LC resonator. The device outputs a digital value that is proportional to frequency. This frequency measurement can be converted to an equivalent capacitance
The FDC is composed of front-end resonant circuit drivers, followed by a multiplexer that sequences through the active channels, connecting them to the core that measures and digitizes the sensor frequency (fSENSOR). The core uses a reference frequency (fREF) to measure the sensor frequency. fREF is derived from either an internal reference clock (oscillator), or an externally supplied clock. The digitized output for each channel is proportional to the ratio of fSENSOR/fREF. The I2C interface is used to support device configuration and to transmit the digitized frequency values to a host processor. The FDC can be placed in shutdown mode, saving current, using the SD pin. The INTB pin may be configured to notify the host of changes in system status.
Figure 12 shows the clock dividers and multiplexers of the FDC.
In Figure 12, the key clocks are fIN, fREF, and fCLK. fCLK is selected from either the internal clock source or external clock source (CLKIN). The frequency measurement reference clock, fREF, is derived from the fCLK source. TI recommends that precision applications use an external master clock that offers the stability and accuracy requirements needed for the application. The internal oscillator may be used in applications that require low cost and do not require high precision. The fINx clock is derived from sensor frequency for a channel x, fSENSORx. fREFx and fINx must meet the requirements listed in Table 1, depending on whether fCLK (master clock) is the internal or external clock.
MODE(1) | CLKIN SOURCE | VALID fREFx RANGE (MHz) | VALID fINx RANGE | SET CHx_FIN_SEL to (2) | SET CHx_SETTLECOUNT to | SET CHx_RCOUNT to |
---|---|---|---|---|---|---|
Multi-channel | Internal | fREFx ≤ 55 | < fREFx /4 | Differential sensor configuration: b01: 0.01MHz to 8.75MHz (divide by 1) b10: 5MHz to 10MHz (divide by 2) Single-ended sensor configuration b10: 0.01MHz to 10MHz (divide by 2) |
> 3 | > 8 |
External | fREFx ≤ 40 | |||||
Single-channel | Either external or internal | fREFx ≤ 35 |
Table 2 shows the clock configuration registers for all channels.
CHANNEL(1) | CLOCK | REGISTER | FIELD [ BIT(S) ] | VALUE |
---|---|---|---|---|
All | fCLK = Master Clock Source | CONFIG, addr 0x1A | REF_CLK_SRC [9] | b0 = internal oscillator is used as the master clock b1 = external clock source is used as the master clock |
0 | fREF0 | CLOCK_DIVIDERS_CH0, addr 0x14 | CH0_FREF_DIVIDER [9:0] | fREF0 = fCLK / CH0_FREF_DIVIDER |
1 | fREF1 | CLOCK_DIVIDERS_CH1, addr 0x15 | CH1_FREF_DIVIDER [9:0] | fREF1 = fCLK / CH1_FREF_DIVIDER |
2 | fREF2 | CLOCK_DIVIDERS_CH2, addr 0x16 | CH2_FREF_DIVIDER [9:0] | fREF2 = fCLK / CH2_FREF_DIVIDER |
3 | fREF3 | CLOCK_DIVIDERS_CH3, addr 0x17 | CH3_FREF_DIVIDER [9:0] | fREF3 = fCLK / CH3_FREF_DIVIDER |
0 | fIN0 | CLOCK_DIVIDERS_CH0, addr 0x14 | CH0_FIN_SEL [13:12] | fIN0 = fSENSOR0 / CH0_FIN_SEL |
1 | fIN1 | CLOCK_DIVIDERS_CH1, addr 0x15 | CH1_FIN_SEL [13:12] | fIN1 = fSENSOR1 / CH1_FIN_SEL |
2 | fIN2 | CLOCK_DIVIDERS_CH2, addr 0x16 | CH2_FIN_SEL [13:12] | fIN2 = fSENSOR2 / CH2_FIN_SEL |
3 | fIN3 | CLOCK_DIVIDERS_CH3, addr 0x17 | CH3_FIN_SEL [13:12] | fIN3 = fSENSOR3 / CH3_FIN_SEL |
The multi-channel package of the FDC enables the user to save board space and support flexible system design. For example, temperature drift can often cause a shift in component values, resulting in a shift in resonant frequency of the sensor. Using a second sensor as a reference provides the capability to cancel out a temperature shift. When operated in multi-channel mode, the FDC sequentially samples the active channels. In single-channel mode, the FDC samples a single channel, which is selectable. Table 3 shows the registers and values that are used to configure either multi-channel or single-channel modes.
MODE | REGISTER | FIELD [ BIT(S) ] | VALUE |
---|---|---|---|
Single channel | CONFIG, addr 0x1A | ACTIVE_CHAN [15:14] | 00 = chan 0 |
01 = chan 1 | |||
10 = chan 2 | |||
11 = chan 3 | |||
MUX_CONFIG addr 0x1B | AUTOSCAN_EN [15] | 0 = continuous conversion on a single channel (default) | |
Multi-channel | MUX_CONFIG addr 0x1B | AUTOSCAN_EN [15] | 1 = continuous conversion on multiple channels |
MUX_CONFIG addr 0x1B | RR_SEQUENCE [14:13] | 00 = Ch0, Ch 1 | |
01 = Ch0, Ch 1, Ch 2 | |||
10 = Ch0, CH1, Ch2, Ch3 |
The digitized sensor measurement for each channel (DATAx) represents the ratio of the sensor frequency to the reference frequency.
The data output (DATAx) of the FDC2112 and FDC2114 is expressed as the 12 MSBs of a 16-bit result:
The data output (DATAx) of the FDC2212 and FDC2214 is expressed as:
Table 4 lists the registers that contain the fixed point sample values for each channel.
CHANNEL(2) | REGISTER(1) | FIELD NAME [ BITS(S) ] AND VALUE (FDC2112, FDC2114) | FIELD NAME [ BITS(S) ] AND VALUE (FDC2212, FDC2214) (3)(4) |
---|---|---|---|
0 | DATA_CH0, addr 0x00 | DATA0 [11:0]: 12 bits of the 16 bit conversion result. 0x000 = under range 0xfff = over range |
DATA0 [27:16]: 12 MSBs of the 28 bit conversion result |
DATA_LSB_CH0, addr 0x01 | Not applicable | DATA0 [15:0]: 16 LSBs of the 28 bit conversion result |
|
1 | DATA_CH1, addr 0x02 | DATA1 [11:0]: 12 bits of the 16 bit conversion result. 0x000 = under range 0xfff = over range |
DATA1 [27:16]: 12 MSBs of the 28 bit conversion result |
DATA_LSB_CH1, addr 0x03 | Not applicable | DATA1 [15:0]: 16 LSBs of the 28 bit conversion result |
|
2 | DATA_CH2, addr 0x04 | DATA2 [11:0]: 12 bits of the 16 bit conversion result. 0x000 = under range 0xfff = over range |
DATA2 [27:16]: 12 MSBs of the 28 bit conversion result |
DATA_LSB_CH2, addr 0x05 | Not applicable | DATA2 [15:0]: 16 LSBs of the 28 bit conversion result |
|
3 | DATA_CH3, addr 0x06 | DATA3 [11:0]: 12 bits of the 16 bit conversion result. 0x000 = under range 0xfff = over range |
DATA3 [27:16]: 12 MSBs of the 28 bit conversion result |
DATA_LSB_CH3, addr 0x07 | Not applicable | DATA3 [15:0]: 16 LSBs of the 28 bit conversion result |
When the FDC sequences through the channels in multi-channel mode, the dwell time interval for each channel is the sum of three parts:
The sensor activation time is the amount of settling time required for the sensor oscillation to stabilize, as shown in Figure 13. The settling wait time is programmable and should be set to a value that is long enough to allow stable oscillation. The settling wait time for channel x is given by:
Table 5 illustrates the registers and values for configuring the settling time for each channel.
CHANNEL(1) | REGISTER | FIELD | CONVERSION TIME(2) |
---|---|---|---|
0 | SETTLECOUNT_CH0, addr 0x10 | CH0_SETTLECOUNT [15:0] | (CH0_SETTLECOUNT*16)/fREF0 |
1 | SETTLECOUNT_CH1, addr 0x11 | CH1_SETTLECOUNT [15:0] | (CH1_SETTLECOUNT*16)/fREF1 |
2 | SETTLECOUNT_CH2, addr 0x12 | CH2_SETTLECOUNT [15:0] | (CH2_SETTLECOUNT*16)/fREF2 |
3 | SETTLECOUNT_CH3, addr 0x13 | CH3_SETTLECOUNT [15:0] | (CH3_SETTLECOUNT*16)/fREF3 |
The SETTLECOUNT for any channel x must satisfy:
where
Round the result to the next highest integer (for example, if Equation 4 recommends a minimum value of 6.08, program the register to 7 or higher).
The conversion time represents the number of reference clock cycles used to measure the sensor frequency. It is set by the CHx_RCOUNT register for the channel. The conversion time for any channel x is:
The reference count value must be chosen to support the required number of effective bits (ENOB). For example, if an ENOB of 13 bits is required, then a minimum conversion time of 213 = 8192 clock cycles is required. 8192 clock cycles correspond to a CHx_RCOUNT value of 0x0200.
CHANNEL | REGISTER | FIELD [ BIT(S) ] | CONVERSION TIME |
---|---|---|---|
0 | RCOUNT_CH0, addr 0x08 | CH0_RCOUNT [15:0] | (CH0_RCOUNT × 16)/fREF0 |
1 | RCOUNT_CH1, addr 0x09 | CH1_RCOUNT [15:0] | (CH1_RCOUNT × 16)/fREF1 |
2 | RCOUNT_CH2, addr 0x0A | CH2_RCOUNT [15:0] | (CH2_RCOUNT × 16)/fREF2 |
3 | RCOUNT_CH3, addr 0x0B | CH3_RCOUNT [15:0] | (CH3_RCOUNT × 16)/fREF3 |
The typical channel switch delay time between the end of conversion and the beginning of sensor activation of the subsequent channel is:
The deterministic conversion time of the FDC allows data polling at a fixed interval. For example, if the programmed SETTLECOUNT is 128 FREF cycles (SETTLECOUNT = 0x0008) and RCOUNT is 512 FREF cycles (RCOUNT=0x0020), then one conversion takes 3.2 ms (sensor-activation time) + 12.8ms (conversion time) + 0.8µs (channel-switch delay) = 16.0 ms per channel. If the FDC is configured for dual-channel operation by setting AUTOSCAN_EN = 1 and RR_SEQUENCE = 00, then one full set of conversion results will be available from the data registers every 32 ms.
A data ready flag (DRDY) is also available for interrupt driven system designs (see the STATUS register description in Register Maps).
The FDC2112 and FDC2114 have internal 16-bit data converters, but the standard conversion output word width is only 12 bits; therefore only 12 of the 16 bits are available from the data registers. By default, the gain feature is disabled and the DATA registers contain the 12 MSBs of the 16-bit word. However, it is possible to shift the data output by up to 4 bits. Figure 15 shows the segment of the 16-bit sample that is reported for each possible gain setting.
For systems in which the sensor signal variation is less than 25% of the full-scale range, the FDC can report conversion results with higher resolution by setting the output gain. the output gain is applied to all device channels. An output gain can be used to apply a 2-bit, 3-bit, or 4-bit shift to the output code for all channels, allowing access to the 4 LSBs of the original 16-bit result. The MSBs of the sample are shifted out when a gain is applied. Do not use the output gain if the MSBs of any active channel are toggling, as the MSBs for that channel will be lost when gain is applied.
Example: If the conversion result for a channel is 0x07A3, with OUTPUT_GAIN = 0x0, the reported output code is 0x07A. If OUTPUT_GAIN is set to 0x3 in the same condition, then the reported output code is 0x7A3. The original 4 MSBs (0x0) are no longer accessible.
CHANNEL(1) | REGISTER | FIELD [ BIT(S) ] | VALUES | EFFECTIVE RESOLUTION (BITS) | OUTPUT RANGE |
---|---|---|---|---|---|
All | RESET_DEV, addr 0x1C | OUTPUT_GAIN [ 10:9 ] | 00 (default): Gain =1 (0 bits shift) | 12 | 100% full scale |
01: Gain = 4 (2 bits left shift) | 14 | 25% full scale | |||
10: Gain = 8 (3 bits left shift) | 15 | 12.5% full scale | |||
11 : Gain = 16 (4 bits left shift) | 16 | 6.25% full scale |
An offset value may be subtracted from each DATA value to compensate for a frequency offset or maximize the dynamic range of the sample data. The offset values should be < fSENSORx_MIN / fREFx. Otherwise, the offset might be so large that it masks the LSBs which are changing.
CHANNEL(1) | REGISTER | FIELD [ BIT(S) ] | VALUE |
---|---|---|---|
0 | OFFSET_CH0, addr 0x0C | CH0_OFFSET [ 15:0 ] | fOFFSET0 = CH0_OFFSET × (fREF0/216) |
1 | OFFSET_CH1, addr 0x0D | CH1_OFFSET [ 15:0 ] | fOFFSET1 = CH1_OFFSET × (fREF1/216) |
2 | OFFSET_CH2, addr 0x0E | CH2_OFFSET [ 15:0 ] | fOFFSET2 = CH2_OFFSET × (fREF2/216) |
3 | OFFSET_CH3, addr 0x0F | CH3_OFFSET [ 15:0 ] | fOFFSET3 = CH3_OFFSET × (fREF3/216) |
The sensor capacitance CSENSE of a differential sensor configuration can be determined by:
where
The FDC2112 and FDC2114 sensor frequency fSENSORx can be determined by:
where
The FDC2212 and FDC2214 sensor frequency fSENSORx can be determined by:
where
The registers listed in Table 9 are used to control the sensor drive current. The recommendations listed in the last column of the table should be followed.
CHANNEL(1) | REGISTER | FIELD [ BIT(S) ] | VALUE |
---|---|---|---|
All | CONFIG, addr 0x1A | SENSOR_ACTIVATE_SEL [11] | Sets current drive for sensor activation. Recommended value is b0 (full current mode). |
0 | CONFIG, addr 0x1A | HIGH_CURRENT_DRV [6] | b0 = normal current drive (1.5 mA) b1 = Increased current drive (> 1.5 mA) for Ch 0 in single channel mode only. Cannot be used in multi-channel mode. |
0 | DRIVE_CURRENT_CH0, addr 0x1E | CH0_IDRIVE [15:11] | Drive current used during the settling and conversion time for Ch. 0. Set such that 1.2 V ≤ sensor oscillation amplitude (pk) ≤ 1.8 V |
1 | DRIVE_CURRENT_CH1, addr 0x1F | CH1_IDRIVE [15:11] | Drive current used during the settling and conversion time for Ch. 1. Set such that 1.2 V ≤ sensor oscillation amplitude (pk) ≤ 1.8 V |
2 | DRIVE_CURRENT_CH2, addr 0x20 | CH2_IDRIVE [15:11] | Drive current used during the settling and conversion time for Ch. 2. Set such that 1.2 V ≤ sensor oscillation amplitude (pk) ≤ 1.8 V |
3 | DRIVE_CURRENT_CH3, addr 0x21 | CH3_IDRIVE [15:11] | Drive current used during the settling and conversion time for Ch. 3 . Set such that 1.2 V ≤ sensor oscillation amplitude (pk) ≤ 1.8 V |
The CHx_IDRIVE field should be programmed such that the sensor oscillates at an amplitude between 1.2 Vpk (VSENSORMIN) and 1.8 Vpk (VSENSORMAX). An IDRIVE value of 00000 corresponds to 16 µA, and IDRIVE = b11111 corresponds to 1563 µA.
A high sensor current drive mode can be enabled to drive sensor coils with > 1.5mA on channel 0, only in single channel mode. This feature can be used when the sensor minimum recommended oscillation amplitude of 1.2V cannot be achieved with the highest IDRIVE setting. Set the HIGH_CURRENT_DRV register bit to b1 to enable this mode.
The registers listed in Table 10 may be used to read device status.
CHANNEL(1) | REGISTER | FIELDS [ BIT(S) ] | VALUES |
---|---|---|---|
All | STATUS, addr 0x18 | 12 fields are available that contain various status bits [ 15:0 ] | Refer to Register Maps for a description of the individual status bits. |
All | STATUS_CONFIG, addr 0x19 | 12 fields are available that are used to configure status reporting [ 15:0 ] | Refer to Register Maps for a description of the individual error configuration bits. |
See the STATUS and STATUS_CONFIG register description in Register Maps. These registers can be configured to trigger an interrupt on the INTB pin for certain events. The following conditions must be met:
When a bit field in the STATUS register is set, the entire STATUS register content is held until read or until the DATA_CHx register is read. Reading also de-asserts INTB.
Interrupts are cleared by one of the following events:
Setting register CONFIG.INTB_DIS to b1 disables the INTB function and holds the INTB pin high.
The input deglitch filter suppresses EMI and ringing above the sensor frequency. It does not impact the conversion result as long as its bandwidth is configured to be above the maximum sensor frequency. The input deglitch filter can be configured in MUX_CONFIG.DEGLITCH register field as shown in Table 11. For optimal performance, TI recommends selection of the lowest setting that exceeds the sensor oscillation frequency. For example, if the maximum sensor frequency is 2 MHz, choose MUX_CONFIG.DEGLITCH = b100 (3.3 MHz).
CHANNEL(1) | MUX_CONFIG.DEGLITCH (addr 0x1B) REGISTER VALUE | DEGLITCH FREQUENCY |
---|---|---|
ALL | 001 | 1 MHz |
ALL | 100 | 3.3 MHz |
ALL | 101 | 10 MHz |
ALL | 011 | 33 MHz |
When the FDC powers up, it enters into sleep mode and waits for configuration. Once the device is configured, exit sleep mode by setting CONFIG.SLEEP_MODE_EN to b0.
TI recommends configuring the FDC while in sleep mode. If a setting on the FDC needs to be changed, return the device to sleep mode, change the appropriate register, and then exit sleep mode.
When operating in the normal (conversion) mode, the FDC is periodically sampling the frequency of the sensor(s) and generating sample outputs for the active channel(s).
Sleep mode is entered by setting the CONFIG.SLEEP_MODE_EN register field to 1. While in this mode, the device configuration is maintained. To exit sleep mode, set the CONFIG.SLEEP_MODE_EN register field to 0. After setting CONFIG.SLEEP_MODE_EN to b0, sensor activation for the first conversion begins after 16,384 fINT clock cycles. While in sleep mode the I2C interface is functional so that register reads and writes can be performed. While in sleep mode, no conversions are performed. In addition, entering sleep mode will clear conversion results, any error condition, and de-assert the INTB pin.
When the SD pin is set to high, the FDC enters shutdown mode. Shutdown mode is the lowest power state. To exit shutdown mode, set the SD pin to low. Entering shutdown mode returns all registers to their default state.
While in shutdown mode, no conversions are performed. In addition, entering shutdown mode clears any error condition and de-assert the INTB pin. While the device is in shutdown mode, is not possible to read to or write from the device via the I2C interface.
The FDC can be reset by writing to RESET_DEV.RESET_DEV. Any active conversion stops, and all register values return to their default value. This register bit always returns 0b when read.
The FDC device uses an I2C interface to access control and data registers.
The FDC uses an extended start sequence with I2C for register access. The maximum speed of the I2C interface is 400 kbit/s. This sequence follows the standard I2C 7-bit slave address followed by an 8-bit pointer register byte to set the register address. When the ADDR pin is set low, the FDC I2C address is 0x2A; when the ADDR pin is set high, the FDC I2C address is 0x2B. The ADDR pin must not change state after the FDC exits Shutdown Mode.
Fields indicated with Reserved must be written only with indicated values, otherwise improper device operation may occur. The R/W column indicates the Read-Write status of the corresponding field. A ‘R/W’ entry indicates read and write capability, a ‘R’ indicates read-only, and a ‘W’ indicates write-only.
ADDRESS | NAME | DEFAULT VALUE | DESCRIPTION |
---|---|---|---|
0x00 | DATA_CH0 | 0x0000 | Channel 0 Conversion Result and status (FDC2112 / FDC2114 only) |
0x0000 | Channel 0 MSB Conversion Result and status (FDC2212 / FDC2214 only) | ||
0x01 | DATA_LSB_CH0 | 0x0000 | Channel 0 LSB Conversion Result. Must be read after Register address 0x00 (FDC2212 / FDC2214 only) |
0x02 | DATA_CH1 | 0x0000 | Channel 1 Conversion Result and status (FDC2112 / FDC2114 only) |
0x0000 | Channel 1 MSB Conversion Result and status (FDC2212 / FDC2214 only) | ||
0x03 | DATA_LSB_CH1 | 0x0000 | Channel 1 LSB Conversion Result. Must be read after Register address 0x02 (FDC2212 / FDC2214 only) |
0x04 | DATA_CH2 | 0x0000 | Channel 2 Conversion Result and status (FDC2114 only) |
0x0000 | Channel 2 MSB Conversion Result and status (FDC2214 only) | ||
0x05 | DATA_LSB_CH2 | 0x0000 | Channel 2 LSB Conversion Result. Must be read after Register address 0x04 (FDC2214 only) |
0x06 | DATA_CH3 | 0x0000 | Channel 3 Conversion Result and status (FDC2114 only) |
0x0000 | Channel 3 MSB Conversion Result and status (FDC2214 only) | ||
0x07 | DATA_LSB_CH3 | 0x0000 | Channel 3 LSB Conversion Result. Must be read after Register address 0x06 (FDC2214 only) |
0x08 | RCOUNT_CH0 | 0x0080 | Reference Count setting for Channel 0 |
0x09 | RCOUNT_CH1 | 0x0080 | Reference Count setting for Channel 1 |
0x0A | RCOUNT_CH2 | 0x0080 | Reference Count setting for Channel 2 (FDC2114 / FDC2214 only) |
0x0B | RCOUNT_CH3 | 0x0080 | Reference Count setting for Channel 3 (FDC2114 / FDC2214 only) |
0x0C | OFFSET_CH0 | 0x0000 | Offset value for Channel 0 (FDC2112 / FDC2114 only) |
0x0D | OFFSET_CH1 | 0x0000 | Offset value for Channel 1 (FDC2112 / FDC2114 only) |
0x0E | OFFSET_CH2 | 0x0000 | Offset value for Channel 2 (FDC2114 only) |
0x0F | OFFSET_CH3 | 0x0000 | Offset value for Channel 3 (FDC2114 only) |
0x10 | SETTLECOUNT_CH0 | 0x0000 | Channel 0 Settling Reference Count |
0x11 | SETTLECOUNT_CH1 | 0x0000 | Channel 1 Settling Reference Count |
0x12 | SETTLECOUNT_CH2 | 0x0000 | Channel 2 Settling Reference Count (FDC2114 / FDC2214 only) |
0x13 | SETTLECOUNT_CH3 | 0x0000 | Channel 3 Settling Reference Count (FDC2114 / FDC2214 only) |
0x14 | CLOCK_DIVIDERS_CH0 | 0x0000 | Reference divider settings for Channel 0 |
0x15 | CLOCK_DIVIDERS_CH1 | 0x0000 | Reference divider settings for Channel 1 |
0x16 | CLOCK_DIVIDERS_CH2 | 0x0000 | Reference divider settings for Channel 2 (FDC2114 / FDC2214 only) |
0x17 | CLOCK_DIVIDERS_CH3 | 0x0000 | Reference divider settings for Channel 3 (FDC2114 / FDC2214 only) |
0x18 | STATUS | 0x0000 | Device Status Reporting |
0x19 | STATUS_CONFIG | 0x0000 | Device Status Reporting Configuration |
0x1A | CONFIG | 0x2801 | Conversion Configuration |
0x1B | MUX_CONFIG | 0x020F | Channel Multiplexing Configuration |
0x1C | RESET_DEV | 0x0000 | Reset Device |
0x1E | DRIVE_CURRENT_CH0 | 0x0000 | Channel 0 sensor current drive configuration |
0x1F | DRIVE_CURRENT_CH1 | 0x0000 | Channel 1 sensor current drive configuration |
0x20 | DRIVE_CURRENT_CH2 | 0x0000 | Channel 2 sensor current drive configuration (FDC2114 / FDC2214 only) |
0x21 | DRIVE_CURRENT_CH3 | 0x0000 | Channel 3 sensor current drive configuration (FDC2114 / FDC2214 only) |
0x7E | MANUFACTURER_ID | 0x5449 | Manufacturer ID |
0x7F | DEVICE_ID | 0x3054 | Device ID (FDC2112, FDC2114 only) |
0x3055 | Device ID (FDC2212, FDC2214 only) |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | CH0_ERR_WD | CH0_ERR_AW | DATA0 | ||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
DATA0 | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:14 | RESERVED | R | 00 | Reserved. |
13 | CH0_ERR_WD | R | 0 | Channel 0 Conversion Watchdog Timeout Error Flag. Cleared by reading the bit. |
12 | CH0_ERR_AW | R | 0 | Channel 0 Amplitude Warning. Cleared by reading the bit. |
11:0 | DATA0 (FDC2112 / FDC2114 only) | R | 0000 0000 0000 | Channel 0 Conversion Result |
DATA0[27:16] (FDC2212 / FDC2214 only) |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
DATA0 | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
DATA0 | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:0 | DATA0[15:0] | R | 0000 0000 0000 | Channel 0 Conversion Result |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | CH1_ERR_WD | CH1_ERR_AW | DATA1 | ||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
DATA1 | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:14 | RESERVED | R | 00 | Reserved. |
13 | CH1_ERR_WD | R | 0 | Channel 1 Conversion Watchdog Timeout Error Flag. Cleared by reading the bit. |
12 | CH1_ERR_AW | R | 0 | Channel 1 Amplitude Warning. Cleared by reading the bit. |
11:0 | DATA1 (FDC2112 / FDC2114 only) | R | 0000 0000 0000 | Channel 1 Conversion Result |
DATA1[27:16] (FDC2212 / FDC2214 only) |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
DATA1 | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
DATA1 | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:0 | DATA1[15:0] | R | 0000 0000 0000 | Channel 1 Conversion Result |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | CH2_ERR_WD | CH2_ERR_AW | DATA2 | ||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
DATA2 | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:14 | RESERVED | R | 00 | Reserved. |
13 | CH2_ERR_WD | R | 0 | Channel 2 Conversion Watchdog Timeout Error Flag. Cleared by reading the bit. |
12 | CH2_ERR_AW | R | 0 | Channel 2 Amplitude Warning. Cleared by reading the bit. |
11:0 | DATA2 (FDC2112 / FDC2114 only) | R | 0000 0000 0000 | Channel 2 Conversion Result |
DATA2[27:16] (FDC2212 / FDC2214 only) |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
DATA2 | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
DATA2 | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:0 | DATA2[15:0] | R | 0000 0000 0000 | Channel 2 Conversion Result |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | CH3_ERR_WD | CH3_ERR_AW | DATA3 | ||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
DATA3 | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:14 | RESERVED | R | 00 | Reserved. |
13 | CH3_ERR_WD | R | 0 | Channel 3 Conversion Watchdog Timeout Error Flag. Cleared by reading the bit. |
12 | CH3_ERR_AW | R | 0 | Channel 3 Amplitude Warning. Cleared by reading the bit. |
11:0 | DATA3 (FDC2112 / FDC2114 only) | R | 0000 0000 0000 | Channel 3 Conversion Result |
DATA3[27:16] (FDC2212 / FDC2214 only) |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
DATA3 | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
DATA3 | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:0 | DATA3[15:0] | R | 0000 0000 0000 | Channel 3 Conversion Result |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
CH0_RCOUNT | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
CH0_RCOUNT | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:0 | CH0_RCOUNT | R/W | 0000 0000 1000 0000 | Channel 0 Reference Count Conversion Interval Time 0x0000-0x00FF: Reserved 0x0100-0xFFFF: Conversion Time (tC0) = (CH0_RCOUNTË£16)/fREF0 |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
CH1_RCOUNT | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
CH1_RCOUNT | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:0 | CH1_RCOUNT | R/W | 0000 0000 1000 0000 | Channel 1 Reference Count Conversion Interval Time 0x0000-0x00FF: Reserved 0x0100-0xFFFF: Conversion Time (tC1)= (CH1_RCOUNTË£16)/fREF1 |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
CH2_RCOUNT | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
CH2_RCOUNT | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:0 | CH2_RCOUNT | R/W | 0000 0000 1000 0000 | Channel 2 Reference Count Conversion Interval Time 0x0000-0x00FF: Reserved 0x0100-0xFFFF: Conversion Time (tC2)= (CH2_RCOUNTË£16)/fREF2 |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
CH3_RCOUNT | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
CH3_RCOUNT | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:0 | CH3_RCOUNT | R/W | 0000 0000 1000 0000 | Channel 3 Reference Count Conversion Interval Time 0x0000-0x00FF: Reserved 0x0100-0xFFFF: Conversion Time (tC3)= (CH3_RCOUNTË£16)/fREF3 |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
CH0_OFFSET | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
CH0_OFFSET | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:0 | CH0_OFFSET | R/W | 0000 0000 0000 0000 | Channel 0 Conversion Offset. fOFFSET_0 = (CH0_OFFSET/216)*fREF0 |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
CH1_OFFSET | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
CH1_OFFSET | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:0 | CH1_OFFSET | R/W | 0000 0000 0000 0000 | Channel 1 Conversion Offset. fOFFSET_1 = (CH1_OFFSET/216)*fREF1 |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
CH2_OFFSET | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
CH2_OFFSET | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:0 | CH2_OFFSET | R/W | 0000 0000 0000 0000 | Channel 2 Conversion Offset. fOFFSET_2 = (CH2_OFFSET/216)*fREF2 |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
CH3_OFFSET | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
CH3_OFFSET | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:0 | CH3_OFFSET | R/W | 0000 0000 0000 0000 | Channel 3 Conversion Offset. fOFFSET_3 = (CH3_OFFSET/216)*fREF3 |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
CH0_SETTLECOUNT | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
CH0_SETTLECOUNT | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:0 | CH0_SETTLECOUNT | R/W | 0000 0000 0000 0000 | Channel 0 Conversion Settling The FDC will use this settling time to allow the LC sensor to stabilize before initiation of a conversion on Channel 0. If the amplitude has not settled prior to the conversion start, an Amplitude warning will be generated if reporting of this type of warning is enabled. 0x0000: Settle Time (tS0)= 32 ÷ fREF0 0x0001: Settle Time (tS0)= 32 ÷ fREF0 0x0002 - 0xFFFF: Settle Time (tS0)= (CH0_SETTLECOUNTË£16) ÷ fREF0 |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
CH1_SETTLECOUNT | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
CH1_SETTLECOUNT | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:0 | CH1_SETTLECOUNT | R/W | 0000 0000 0000 0000 | Channel 1 Conversion Settling The FDC will use this settling time to allow the LC sensor to stabilize before initiation of a conversion on a Channel 1. If the amplitude has not settled prior to the conversion start, an Amplitude warning will be generated if reporting of this type of warning is enabled. 0x0000: Settle Time (tS1)= 32 ÷ fREF1 0x0001: Settle Time (tS1)= 32 ÷ fREF1 0x0002 - 0xFFFF: Settle Time (tS1)= (CH1_SETTLECOUNTË£16) ÷ fREF1 |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
CH2_SETTLECOUNT | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
CH2_SETTLECOUNT | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:0 | CH2_SETTLECOUNT | R/W | 0000 0000 0000 0000 | Channel 2 Conversion Settling The FDC will use this settling time to allow the LC sensor to stabilize before initiation of a conversion on Channel 2. If the amplitude has not settled prior to the conversion start, an Amplitude warning will be generated if reporting of this type of warning is enabled. 0x0000: Settle Time (tS2) = 32 ÷ fREF2 0x0001: Settle Time (tS2) = 32 ÷ fREF2 0x0002 - 0xFFFF: Settle Time (tS2)= (CH2_SETTLECOUNTË£16) ÷ fREF2 |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
CH3_SETTLECOUNT | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
CH3_SETTLECOUNT | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:0 | CH3_SETTLECOUNT | R/W | 0000 0000 0000 0000 | Channel 3 Conversion Settling The FDC will use this settling time to allow the LC sensor to stabilize before initiation of a conversion on Channel 3. If the amplitude has not settled prior to the conversion start, an Amplitude warning will be generated if reporting of this type of warning is enabled 0x0000: Settle Time (tS3) = 32 ÷ fREF3 0x0001: Settle Time (tS3) = 32 ÷ fREF3 0x0002 - 0xFFFF: Settle Time (tS3)= (CH3_SETTLECOUNTË£16) ÷ fREF3 |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | CH0_FIN_SEL | RESERVED | CH0_FREF_DIVIDER | ||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
CH0_FREF_DIVIDER | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:14 | RESERVED | R/W | 00 | Reserved. Set to b00. |
13:12 | CH0_FIN_SEL | R/W | 00 | Channel 0 Sensor frequency select for differential sensor configuration: b01: divide by 1. Choose for sensor frequencies between 0.01 MHz and 8.75 MHz b10: divide by 2. Choose for sensor frequencies between 5 MHz and 10 MHz for single-ended sensor configuration: b10: divide by 2. Choose for sensor frequencies between 0.01 MHz and 10 MHz |
11:10 | RESERVED | R/W | 00 | Reserved. Set to b00. |
9:0 | CH0_FREF_DIVIDER | R/W | 00 0000 0000 | Channel 0 Reference Divider Sets the divider for Channel 0 reference. Use this to scale the maximum conversion frequency. b00’0000’0000: Reserved. Do not use. CH0_FREF_DIVIDER≥b00’0000’0001: fREF0 = fCLK/CH0_FREF_DIVIDER |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | CH1_FIN_SEL | RESERVED | CH1_FREF_DIVIDER | ||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
CH1_FREF_DIVIDER | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:14 | RESERVED | R/W | 00 | Reserved. Set to b00. |
13:12 | CH1_FIN_SEL | R/W | 0000 | Channel 1 Sensor frequency select for differential sensor configuration: b01: divide by 1. Choose for sensor frequencies between 0.01 MHz and 8.75 MHz b10: divide by 2. Choose for sensor frequencies between 5 MHz and 10 MHz for single-ended sensor configuration: b10: divide by 2. Choose for sensor frequencies between 0.01 MHz and 10 MHz |
11:10 | RESERVED | R/W | 00 | Reserved. Set to b00. |
9:0 | CH1_FREF_DIVIDER | R/W | 00 0000 0000 | Channel 1 Reference Divider Sets the divider for Channel 1 reference. Use this to scale the maximum conversion frequency. b00’0000’0000: Reserved. Do not use. CH1_FREF_DIVIDER≥ b00’0000’0001: fREF1 = fCLK/CH1_FREF_DIVIDER |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | CH2_FIN_SEL | RESERVED | CH2_FREF_DIVIDER | ||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
CH2_FREF_DIVIDER | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:14 | RESERVED | R/W | 00 | Reserved. Set to b00. |
13:12 | CH2_FIN_SEL | R/W | 0000 | Channel 2 Sensor frequency select for differential sensor configuration: b01: divide by 1. Choose for sensor frequencies between 0.01 MHz and 8.75 MHz b10: divide by 2. Choose for sensor frequencies between 5 MHz and 10 MHz for single-ended sensor configuration: b10: divide by 2. Choose for sensor frequencies between 0.01 MHz and 10 MHz |
11:10 | RESERVED | R/W | 00 | Reserved. Set to b00. |
9:0 | CH2_FREF_DIVIDER | R/W | 00 0000 0000 | Channel 2 Reference Divider Sets the divider for Channel 2 reference. Use this to scale the maximum conversion frequency. b00’0000’0000: Reserved. Do not use. CH2_FREF_DIVIDER ≥ b00’0000’0001: fREF2 = fCLK/CH2_FREF_DIVIDER |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | CH3_FIN_SEL | RESERVED | CH3_FREF_DIVIDER | ||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
CH3_FREF_DIVIDER | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:14 | RESERVED | R/W | 00 | Reserved. Set to b00. |
13:12 | CH3_FIN_SEL | R/W | 0000 | Channel 3 Sensor frequency select for differential sensor configuration: b01: divide by 1. Choose for sensor frequencies between 0.01 MHz and 8.75 MHz b10: divide by 2. Choose for sensor frequencies between 5 MHz and 10 MHz for single-ended sensor configuration: b10: divide by 2. Choose for sensor frequencies between 0.01 MHz and 10 MHz |
11:10 | RESERVED | R/W | 00 | Reserved. Set to b00. |
9:0 | CH3_FREF_DIVIDER | R/W | 00 0000 0000 | Channel 3 Reference Divider Sets the divider for Channel 3 reference. Use this to scale the maximum conversion frequency. b00’0000’0000: reserved CH3_FREF_DIVIDER ≥ b00’0000’0001: fREF3 = fCLK/CH3_FREF_DIVIDER |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
ERR_CHAN | RESERVED | ERR_WD | RESERVED | ||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | DRDY | RESERVED | CH0_UNREADCONV | CH1_ UNREADCONV | CH2_ UNREADCONV | CH3_ UNREADCONV | |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:14 | ERR_CHAN | R | 00 | Error Channel Indicates which channel has generated a Flag or Error. Once flagged, any reported error is latched and maintained until either the STATUS register or the DATA_CHx register corresponding to the Error Channel is read. b00: Channel 0 is source of flag or error. b01: Channel 1 is source of flag or error. b10: Channel 2 is source of flag or error (FDC2114, FDC2214 only). b11: Channel 3 is source of flag or error (FDC2114, FDC2214 only). |
13:12 | RESERVED | R | 00 | Reserved |
11 | ERR_WD | R | 0 | Watchdog Timeout Error b0: No Watchdog Timeout error was recorded since the last read of the STATUS register. b1: An active channel has generated a Watchdog Timeout error. Refer to STATUS.ERR_CHAN field to determine which channel is the source of this error. |
10 | ERR_AHW | R | 0 | Amplitude High Warning b0: No Amplitude High warning was recorded since the last read of the STATUS register. b1: An active channel has generated an Amplitude High warning. Refer to STATUS.ERR_CHAN field to determine which channel is the source of this warning. |
9 | ERR_ALW | R | 0 | Amplitude Low Warning b0: No Amplitude Low warning was recorded since the last read of the STATUS register. b1: An active channel has generated an Amplitude Low warning. Refer to STATUS.ERR_CHAN field to determine which channel is the source of this warning. |
8:7 | RESERVED | R | 00 | Reserved |
6 | DRDY | R | 0 | Data Ready Flag. b0: No new conversion result was recorded in the STATUS register. b1: A new conversion result is ready. When in Single Channel Conversion, this indicates a single conversion is available. When in sequential mode, this indicates that a new conversion result for all active channels is now available. |
3 | CH0_UNREADCONV | R | 0 | Channel 0 Unread Conversion b0: No unread conversion is present for Channel 0. b1: An unread conversion is present for Channel 0. Read Register DATA_CH0 to retrieve conversion results. |
2 | CH1_ UNREADCONV | R | 0 | Channel 1 Unread Conversion b0: No unread conversion is present for Channel 1. b1: An unread conversion is present for Channel 1. Read Register DATA_CH1 to retrieve conversion results. |
1 | CH2_ UNREADCONV | R | 0 | Channel 2 Unread Conversion b0: No unread conversion is present for Channel 2. b1: An unread conversion is present for Channel 2. Read Register DATA_CH2 to retrieve conversion results (FDC2114, FDC2214 only) |
0 | CH3_ UNREADCONV | R | 0 | Channel 3 Unread Conversion b0: No unread conversion is present for Channel 3. b1: An unread conversion is present for Channel 3. Read Register DATA_CH3 to retrieve conversion results (FDC2114, FDC2214 only) |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | WD_ ERR2OUT | AH_WARN2OUT | AL_WARN2OUT | RESERVED | |||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | WD_ERR2INT | RESERVED | DRDY_2INT | ||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:14 | RESERVED | R/W | 00 | Reserved (set to b000) |
13 | WD_ ERR2OUT | R/W | 0 | Watchdog Timeout Error to Output Register b0: Do not report Watchdog Timeout errors in the DATA_CHx registers. b1: Report Watchdog Timeout errors in the DATA_CHx.CHx_ERR_WD register field corresponding to the channel that generated the error. |
12 | AH_WARN2OUT | R/W | 0 | Amplitude High Warning to Output Register b0:Do not report Amplitude High warnings in the DATA_CHx registers. b1: Report Amplitude High warnings in the DATA_CHx.CHx_ERR_AW register field corresponding to the channel that generated the warning. |
11 | AL_WARN2OUT | R/W | 0 | Amplitude Low Warning to Output Register b0: Do not report Amplitude Low warnings in the DATA_CHx registers. b1: Report Amplitude High warnings in the DATA_CHx.CHx_ERR_AW register field corresponding to the channel that generated the warning. |
10:6 | RESERVED | R/W | 0 0000 | Reserved (set to b0 0000) |
5 | WD_ERR2INT | R/W | 0 | Watchdog Timeout Error to INTB b0: Do not report Under-range errors by asserting INTB pin and STATUS register. b1: Report Watchdog Timeout errors by asserting INTB pin and updating STATUS.ERR_WD register field. |
4:1 | Reserved | R/W | 0000 | Reserved (set to b000) |
0 | DRDY_2INT | R/W | 0 | Data Ready Flag to INTB b0: Do not report Data Ready Flag by asserting INTB pin and STATUS register. b1: Report Data Ready Flag by asserting INTB pin and updating STATUS. DRDY register field. |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
ACTIVE_CHAN | SLEEP_MODE_EN | RESERVED | SENSOR_ACTIVATE_SEL | RESERVED | REF_CLK_SRC | RESERVED | |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
INTB_DIS | HIGH_CURRENT_DRV | RESERVED | |||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:14 | ACTIVE_CHAN | R/W | 00 | Active channel selection Selects channel for continuous conversions when MUX_CONFIG.SEQUENTIAL is 0. b00: Perform continuous conversions on Channel 0 b01: Perform continuous conversions on Channel 1 b10: Perform continuous conversions on Channel 2 (FDC2114, FDC2214 only) b11: Perform continuous conversions on Channel 3 (FDC2114, FDC2214 only) |
13 | SLEEP_MODE_EN | R/W | 1 | Sleep mode enable Enter or exit low power sleep mode. b0: Device is active. b1: Device is in sleep mode. |
12 | RESERVED | R/W | 0 | Reserved. Set to b1. |
11 | SENSOR_ACTIVATE_SEL | R/W | 1 | Sensor activation mode selection. Set the mode for sensor initialization. b0: Full current activation mode – the FDC will drive maximum sensor current for a shorter sensor activation time. b1: Low power activation mode – the FDC uses the value programmed in DRIVE_CURRENT_CHx during sensor activation to minimize power consumption. |
10 | RESERVED | R/W | 0 | Reserved. Set to b1. |
9 | REF_CLK_SRC | R/W | 0 | Select Reference Frequency Source b0: Use Internal oscillator as reference frequency b1: Reference frequency is provided from CLKIN pin. |
8 | RESERVED | R/W | 0 | Reserved. Set to b0. |
7 | INTB_DIS | R/W | 0 | INTB Disable b0: INTB pin is asserted when status register updates. b1: INTB pin is not asserted when status register updates |
6 | HIGH_CURRENT_DRV | R/W | 0 | High Current Sensor Drive b0: The FDC drives all channels with normal sensor current (1.5 mA maximum). b1: The FDC drives channel 0 with current >1.5 mA. This mode is not supported if AUTOSCAN_EN = b1 (multi-channel mode) |
5:0 | RESERVED | R/W | 00 0001 | Reserved Set to b00’0001 |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
AUTOSCAN_EN | RR_SEQUENCE | RESERVED | |||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | DEGLITCH | ||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15 | AUTOSCAN_EN | R/W | 0 | Auto-Scan mode enable b0: Continuous conversion on the single channel selected by CONFIG.ACTIVE_CHAN register field. b1: Auto-Scan conversions as selected by MUX_CONFIG.RR_SEQUENCE register field. |
14:13 | RR_SEQUENCE | R/W | 00 | Auto-Scan sequence configuration Configure multiplexing channel sequence. The FDC performs a single conversion on each channel in the sequence selected, and then restart the sequence continuously. b00: Ch0, Ch1 b01: Ch0, Ch1, Ch2 (FDC2114, FDC2214 only) b10: Ch0, Ch1, Ch2, Ch3 (FDC2114, FDC2214 only) b11: Ch0, Ch1 |
12:3 | RESERVED | R/W | 00 0100 0001 | Reserved. Must be set to 00 0100 0001 |
2:0 | DEGLITCH | R/W | 111 | Input deglitch filter bandwidth. Select the lowest setting that exceeds the oscillation tank oscillation frequency. b001: 1 MHz b100: 3.3 MHz b101: 10 MHz b111: 33 MHz |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESET_DEV | RESERVED | OUTPUT_GAIN | RESERVED | ||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15 | RESET_DEV | R/W | 0 | Device Reset Write b1 to reset the device. Will always readback 0. |
14:11 | RESERVED | R/W | 0000 | Reserved. Set to b0000 |
10:9 | OUTPUT_GAIN | R/W | 00 | Output gain control (FDC2112, FDC2114 only) 00: Gain =1 (0 bits shift) 01: Gain = 4 (2 bits shift) 10: Gain = 8 (3 bits shift) 11: Gain = 16 (4 bits shift) |
8:0 | RESERVED | R/W | 0 0000 0000 | Reserved, Set to b0 0000 0000 |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
CH0_IDRIVE | RESERVED | ||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:11 | CH0_IDRIVE | R/W | 0000 0 | Channel 0 Sensor drive current This field defines the Drive Current used during the settling + conversion time of Channel 0 sensor clock. Set such that 1.2V ≤ sensor oscillation amplitude (pk) ≤ 1.8V 00000: 0.016 mA 00001: 0.018 mA 00010: 0.021 mA 00011: 0.025 mA 00100: 0.028 mA 00101: 0.033 mA 00110: 0.038 mA 00111: 0.044 mA 01000: 0.052 mA 01001: 0.060 mA 01010: 0.069 mA 01011: 0.081 mA 01100: 0.093 mA 01101: 0.108 mA 01110: 0.126 mA 01111: 0.146 mA 10000: 0.169 mA 10001: 0.196 mA 10010: 0.228 mA 10011: 0.264 mA 10100: 0.307 mA 10101: 0.356 mA 10110: 0.413 mA 10111: 0.479 mA 11000: 0.555 mA 11001: 0.644 mA 11010: 0.747 mA 11011: 0.867 mA 11100: 1.006 mA 11101: 1.167 mA 11110: 1.354 mA 11111: 1.571 mA |
10:0 | RESERVED | – | 000 0000 0000 | Reserved |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
CH1_IDRIVE | RESERVED | ||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:11 | CH1_IDRIVE | R/W | 0000 0 | Channel 1 Sensor drive current This field defines the drive current used during the settling + conversion time of Channel 1 sensor clock. Set such that 1.2 V ≤ sensor oscillation amplitude (pk) ≤ 1.8 V 00000: 0.016 mA 00001: 0.018 mA 00010: 0.021 mA ... 11111: 1.571 mA |
10:0 | RESERVED | - | 000 0000 0000 | Reserved |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
CH2_IDRIVE | RESERVED | ||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:11 | CH2_IDRIVE | R/W | 0000 0 | Channel 2 Sensor drive current This field defines the drive current to be used during the settling + conversion time of Channel 2 sensor clock. Set such that 1.2 V ≤ sensor oscillation amplitude (pk) ≤ 1.8 V 00000: 0.016 mA 00001: 0.018 mA 00010: 0.021 mA ... 11111: 1.571 mA |
10:0 | RESERVED | – | 000 0000 0000 | Reserved |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
CH3_IDRIVE | RESERVED | ||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:11 | CH3_IDRIVE | R/W | 0000 0 | Channel 3 Sensor drive current This field defines the drive current to be used during the settling + conversion time of Channel 3 sensor clock. Set such that 1.2V ≤ sensor oscillation amplitude (pk) ≤ 1.8 V 00000: 0.016 mA 00001: 0.018 mA 00010: 0.021 mA ... 11111: 1.571 mA |
10:0 | RESERVED | – | 000 0000 0000 | Reserved |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
MANUFACTURER_ID | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
MANUFACTURER_ID | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15:0 | MANUFACTURER_ID | R | 0101 0100 0100 1001 | Manufacturer ID = 0x5449 |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
DEVICE_ID | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7:0 | DEVICE_ID | R | 0011 0000 0101 0100 | Device ID 0x3054 (FDC2112, FDC2114 only) 0x3055 (FDC2212, FDC2214 only) |