SBOS475K March   2009  – November 2023 INA210-Q1 , INA211-Q1 , INA212-Q1 , INA213-Q1 , INA214-Q1 , INA215-Q1

PRODUCTION DATA  

  1.   1
  2. Features
  3. Applications
  4. Description
  5. Pin Configuration and Functions
  6. Specifications
    1. 5.1 Absolute Maximum Ratings
    2. 5.2 ESD Ratings
    3. 5.3 Recommended Operating Conditions
    4. 5.4 Thermal Information
    5. 5.5 Electrical Characteristics
    6. 5.6 Typical Characteristics
  7. Detailed Description
    1. 6.1 Overview
    2. 6.2 Functional Block Diagram
    3. 6.3 Feature Description
      1. 6.3.1 Basic Connections
      2. 6.3.2 Selecting RS
    4. 6.4 Device Functional Modes
      1. 6.4.1 Input Filtering
      2. 6.4.2 Shutting Down the INA21x-Q1 Series
      3. 6.4.3 REF Input Impedance Effects
      4. 6.4.4 Using the INA21x-Q1 with Common-Mode Transients Above 26 V
      5. 6.4.5 Improving Transient Robustness
  8. Application and Implementation
    1. 7.1 Application Information
    2. 7.2 Typical Applications
      1. 7.2.1 Unidirectional Operation
        1. 7.2.1.1 Design Requirements
        2. 7.2.1.2 Detailed Design Procedure
        3. 7.2.1.3 Application Curve
      2. 7.2.2 Bidirectional Operation
        1. 7.2.2.1 Design Requirements
        2. 7.2.2.2 Detailed Design Procedure
        3. 7.2.2.3 Application Curve
  9. Power Supply Recommendations
  10. Layout
    1. 9.1 Layout Guidelines
    2. 9.2 Layout Example
  11. 10Device and Documentation Support
    1. 10.1 Documentation Support
      1. 10.1.1 Related Documentation
    2. 10.2 Related Links
    3. 10.3 Receiving Notification of Documentation Updates
    4. 10.4 Support Resources
    5. 10.5 Trademarks
    6. 10.6 Electrostatic Discharge Caution
    7. 10.7 Glossary
  12. 11Revision History
  13. 12Mechanical, Packaging, and Orderable Information

Package Options

Mechanical Data (Package|Pins)
Thermal pad, mechanical data (Package|Pins)
Orderable Information

Input Filtering

An obvious and straightforward location for filtering is at the output of the INA21x-Q1 family of devices. However, this location negates the advantage of the low output impedance of the internal buffer. The only other filtering option is at the input pins of the INA21x-Q1 family of devices. This location, however, requires consideration of the ±30% tolerance of the internal resistances. Figure 6-2 shows a filter placed at the input pins.

GUID-4303403C-4D4E-4CB0-970C-B09B3D8BF3BE-low.gifFigure 6-2 Filter at Input Pins

The addition of external series resistance, however, creates an additional error in the measurement so the value of these series resistors must be kept to 10 Ω (or less, if possible) to reduce impact to accuracy. The internal bias network shown in Figure 6-2 that is present at the input pins creates a mismatch in input bias currents when a differential voltage is applied between the input pins. If additional external series filter resistors are added to the circuit, the mismatch in bias currents results in a mismatch of voltage drops across the filter resistors. This mismatch creates a differential error voltage that subtracts from the voltage developed at the shunt resistor. This error results in a voltage at the device input pins that is different than the voltage developed across the shunt resistor. Without the additional series resistance, the mismatch in input bias currents has little effect on device operation. The amount of error these external filter resistors add to the measurement can be calculated using Equation 2 where the gain error factor is calculated using Equation 1.

The amount of variance in the differential voltage present at the device input relative to the voltage developed at the shunt resistor is based both on the external series resistance value as well as the internal input resistors, R3 and R4 (or RINT as shown in Figure 6-2). The reduction of the shunt voltage reaching the device input pins appears as a gain error when comparing the output voltage relative to the voltage across the shunt resistor. A factor can be calculated to determine the amount of gain error that is introduced by the addition of external series resistance. Use Equation 1 to calculate the expected deviation from the shunt voltage to what is measured at the device input pins.

Equation 1. GUID-1986C9B8-651D-40A4-AE4E-77CC2FD5F319-low.gif

where:

  • RINT is the internal input resistor (R3 and R4), and
  • RS is the external series resistance.

With the adjustment factor from Equation 1 including the device internal input resistance, this factor varies with each gain version, as shown in Table 6-1. Table 6-2 lists each individual device gain-error factor.

Table 6-1 Input Resistance
PRODUCTGAINRINT (kΩ)
INA210-Q12005
INA211-Q15002
INA212-Q110001
INA213-Q15020
INA214-Q110010
INA215-Q17513.3
Table 6-2 Device Gain Error Factor
PRODUCTSIMPLIFIED GAIN ERROR FACTOR
INA210-Q1 GUID-F5F982C6-9B6A-48C0-9580-D358CD8DEC84-low.gif
INA211-Q1 GUID-8E9C0F22-268A-4F80-85A9-3C854476F41D-low.gif
INA212-Q1 GUID-01598834-AA9D-4D24-9CFC-1D760AEC95FE-low.gif
INA213-Q1 GUID-FEE82C6C-386F-47AF-86EF-53FF62305DC1-low.gif
INA214-Q1 GUID-701962CF-BB2D-44EB-B309-45AA52CE1372-low.gif
INA215-Q1 GUID-0F779239-24D4-461C-8E41-CB9C46921B56-low.gif

Use Equation 2 to calculate the gain error that can be expected from the addition of the external series resistors.


Equation 2. GUID-0A092707-4731-4945-B32C-94C91EBFA501-low.gif

For example, using an INA212-Q1 device and the corresponding gain error equation from Table 6-2, a series resistance of 10 Ω results in a gain error factor of 0.982. The corresponding gain error is then calculated using Equation 2, resulting in a gain error of approximately 1.77% solely because of the external 10-Ω series resistors. Using an INA213-Q1 with the same 10-Ω series resistor results in a gain error factor of 0.991 and a gain error of 0.84% again solely because of these external resistors.