SBOS576C May 2012 – September 2026 INA3221
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
This design shows two shunt voltage conversion times to demonstrate the difference in the alert response times. This design generates a critical-alert response when the input voltage exceeds 80mV on channel 1. See Table 9-1 for all design parameters.
For the first example the shunt voltage conversion time is set to 1.1ms. When the input signal exceeds 80mV, the Critical alert pin pulls low after the conversion cycle completes, indicating an overcurrent condition, as shown in Figure 9-2.
For the second example, the conversion time is set to 588µs, and the response is shown in Figure 9-3.