SNVS007H september 1998 – june 2023 LM2676
PRODUCTION DATA
Select R1 and R2, as shown in Figure 9-5.
Use the following formula to select the appropriate resistor values.
where
Select a value for R1 between 240 Ω and 1.5 kΩ. The lower resistor values minimize noise pickup in the sensitive feedback pin. (For the lowest temperature coefficient and the best stability with time, use 1% metal film resistors.)
Select R1 to be 1 kΩ, 1%. Solve for R2.
where