SNVSBI7B January 2020 – January 2021 LM5156-Q1 , LM51561-Q1
PRODUCTION DATA
The device provides cycle-by-cycle peak current limit protection that turns off the MOSFET when the sum of the inductor current and the programmable slope compensation ramp reaches the current limit threshold (VCLTH). Peak inductor current limit (IPEAK-CL) in steady state is calculated as shown in Equation 10.

The practical duty cycle is greater than the estimated due to voltage drops across the MOSFET and sense resistor. The estimated duty cycle is calculated as shown in Equation 11.

Boost converters have a natural pass-through path from the supply to the load through the high-side power diode (D1). Because of this path and the minimum on-time limitation of the device, boost converters cannot provide current limit protection when the output voltage is close to or less than the input supply voltage. The minimum on-time is shown in Figure 8-12 and is calculated as Equation 12.

If required, a small external RC filter (RF, CF) at the CS pin can be added to overcome the large leading edge spike of the current sense signal. Select an RF value in the range of 10 Ω to 200 Ω and a CF value in the range of 100 pF to 2 nF. Because of the effect of this RC filter, the peak current limit is not valid when the on-time is less than 2 × RF × CF. To fully discharge the CF during the off-time, the RC time constant should satisfy the following inequality.