SNVSCH3A June 2025 – October 2026 LM65625 , LM65635 , LM65645
PRODUCTION DATA
If an output voltage different from either 3.3V or 5V is required, then the adjustable output voltage mode must be used. In that case, an external voltage divider must be connected between the output node and the FB pin, while Equation 5 and Equation 6 are used to determine the divider values.
Note that Equation 6 states that the parallel combination of RFBB and RFBT must be greater than 4kΩ and less than 100kΩ. This limit is required because the regulator must reliably detect the sate of the FB pin during the start-up sequence to set the output voltage mode correctly. The capacitance from the FB pin to ground must be minimized on the PCB layout.
If the adjustable output voltage mode had been chosen for this example, then values of RFBT = 100kΩ and RFBB = 19.1kΩ satisfy both Equation 5 and Equation 6.
For more details, see Section 7.3.1.