SBOS747C May 2016 – July 2026 REF61
PRODUCTION DATA
The REF6125, REF6130, REF6133 and REF6141 are specified to deliver current load of ±4mA. The REF6145 is specified to deliver ±3.5mA, and the REF6150 is specified to deliver ±3mA. The REF61xx are protected from short circuits at the output by limiting the output short-circuit current.
The short-circuit current limit (ISC) of the REF61xx family of devices is adjusted by connecting a resistor (RSS) on the SS pin. The short-circuit current limit when the REF61xx device is sourcing current can be calculated as shown in Equation 4:

The short circuit current limit when the REF61xx device is sinking is calculated as shown in Equation 5:

The recommended output current of the REF61xx also depends on the resistor connected to the SS pin. The recommended output current (sourcing and sinking) for the REF6125, REF6130, REF6133 and REF6141 is given by Equation 6:

The recommended output current (sourcing and sinking) for the REF6145 is given by Equation 7:

The recommended output current (sourcing and sinking) for the REF6150 is given by Equation 8:

The temperature of the device increases according to Equation 9:

where:
The REF61xx maximum junction temperature must not exceed the absolute maximum rating of 150°C.