SLVSDQ6A July 2018 – November 2018 TL431LI , TL432LI
PRODUCTION DATA.
The dynamic impedance is defined as:
. When the device is operating with two external resistors (see Figure 15), the total dynamic impedance of the circuit is given by:
which is approximately equal to
.
The VKA of the TL431LI can be affected by the dynamic impedance. The TL431LI test current Itest for VKA is specified on the Eletrical Characteristics . Any deviation from Itest can cause deviation on the output VKA. Figure 17 shows the effect of the dynamic impedance on the VKA.
Figure 17. Dynamic Impedance