SCDS486 April 2025 TMUX6612-Q1
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
Source on-leakage current is defined as the leakage current flowing into or out of the source pin when the switch is on. This current is denoted by the symbol IS(ON).
Drain on-leakage current is defined as the leakage current flowing into or out of the drain pin when the switch is on. This current is denoted by the symbol ID(ON).
Either the source pin or drain pin is left floating during the measurement. Figure 16-3 shows the circuit used for measuring the on-leakage current, denoted by IS(ON) or ID(ON).
Figure 16-3 On-Leakage
Measurement Setup