SCDS466A August 2023 – December 2024 TMUX7612
PRODUCTION DATA
For analog switches in many applications, several 100s of mA of current needs to be supported through the switch (from source to drain, or NO/NC to COM). Many devices already have a maximum current specified based on ambient temperature, but if a device specifies with junction temperature or you want to calculate for your specific use case (temperature, supply voltage, channels in parallel) you can use the following equations and scheme.
There are mainly 2 limitations to this maximum current:
To calculate maximum current for your specific setup you need the following information:
Device maximum TJ=150°C
For this example we assume 20°C of self-heating at a maximum TA=105°C and operating with 4 channels at once at ±15V. We can assume worst case RON = 2.2Ω. This number is taken from the maximum specified value at TA = 125°C where TJ=125°C since the specification assumes no self-heating. Using the following equation we can calculate the maximum thermal limitation.
Similarly, you can calculate the TJ and total power dissipated in these examples with the following equations. Note there will be some small power dissipated from the supply current consumption of the device, which is ignored here.
Pulse current can be calculated the same way, but using the duty cycle, d. Typically, pulse current is specified at a 10% duty cycle; however, do not exceed the maximum current provided in the pulse current table even with a shorter duty cycle.