SLVSB49F November 2011 – January 2015 TPS22910A , TPS22912C
PRODUCTION DATA.
This family of devices are single channel, 2-A load switches in ultra-small, space saving 4-pin WCSP package. These devices implement a low resistance P-channel MOSFET with a controlled rise time for applications that need to limit the inrush current.
These devices are designed to have very low leakage current during off state. This prevents downstream circuits from pulling high standby current from the supply. Integrated control logic, driver, power supply, and output discharge FET eliminates the need for additional external components, which reduces solution size and BOM count.

The ON pin controls the state of the switch. The ON pin is compatible with standard GPIO logic threshold. It can be used with any microcontroller with 1.2-V, 1.8-V, 2.5-V, 3.3-V, or 5.5-V GPIO.
Under-voltage lockout protection turns off the switch if the input voltage drops below the under-voltage lockout threshold (UVLO). With the ON pin active, the input voltage rising above the under-voltage lockout threshold will cause a controlled turn-on of the switch to limit current over-shoot.
In a scenario where VOUT is greater than VIN, there is potential for reverse current to flow through the pass FET or the body diode. The devices monitor VIN and VOUT voltage levels. When the reverse current voltage threshold (VRCP) is exceeded, the switch is disabled (within 10μs typ). Additionally, the body diode is disengaged so as to prevent any reverse current flow to VIN. The peak instantaneous reverse current is the current it takes to activate the reverse current protection. After the reverse current protection has activated due to the peak instantaneous reverse current, the DC (off-state) leakage current from VOUT and VIN is referred to as IRCP(leak) (see Figure 49). The pass FET, and the output voltage (VOUT), will resume normal operation when the reverse voltage scenario is no longer present.
The following formula can be used to calculate the amount of peak instantaneous reverse current for a particular application:

Where,
IRC is the amount of reverse current,
rON(VIN) is the on-resistance at the VIN of the reverse current condition.
VRCP is the reverse voltage threshold.
Figure 49. Reverse Current
Table 2 describes what the VOUT pin will be connected to for a particular device as determined by the ON pin
| ON | TPS22910A | TPS22912C | TPS22913B/C |
|---|---|---|---|
| L | VIN | Open | GND |
| H | Open | VIN | VIN |