| 1 |
FLT |
O |
Fault low indicated the fault time has expired and the FET is switched off |
| 2 |
EN |
I |
Device is enabled when this pin is pulled low |
| 3 |
VIN |
I |
Power In and control supply voltage |
| 4 |
GND |
— |
GND |
| 5 |
ISET |
I/O |
A resistor to ground sets the fault current, the current limit is 150% of the fault current |
| 6 |
CT |
I/O |
A capacitor to ground sets the fault time |
| 7 |
VOUT |
O |
Output to the load |
| 8 |
PG |
O |
Power Good low represents the output voltage is within 300 mV of the input voltage |