SNVSCB1D December 2022 – December 2025 TPSM33615 , TPSM33625
PRODUCTION DATA
| PIN | TYPE | DESCRIPTION | ||
|---|---|---|---|---|
| NO. | NAME | |||
| 1 | PGOOD | A | Power-good monitor. Open-drain
output that asserts low if the feedback voltage is not within the specified window
thresholds. A 10-kΩ to 100-kΩ pullup resistor is required to a suitable pullup
voltage. If not used, this pin can be left open or connected to GND. High = power OK, Low = power bad. PGOOD pin goes low when EN = Low. |
|
| 2 | EN | A | Precision enable input pin. High = ON, Low = OFF. Can be connected to VIN. Precision enable allows the pin to be used as an adjustable UVLO. Can be connected directly to VIN. The module can be turned off by using an open-drain or collector device to connect this pin to GND. An external voltage divider can be placed between this pin, GND, and VIN to create an external UVLO.Do not float this pin. | |
| 3 | VIN | P | Input supply voltage. Connect the input supply to these pins. Connect a high-quality bypass capacitor or capacitors directly to this pin and GND in close proximity to the module. Refer to Section 8.5.2 for input capacitor placement example. | |
| 4 | VOUT | P | Output voltage. The pin is connected to the internal output
inductor. Connect the pin to the output load and connect external output
capacitors between the pin and GND. |
|
| 5, 6 | SW | P | Power module switch node. Do not place any external component on this pin or connect to any signal. The amount of copper placed on these pins must be kept to a minimum to prevent issues with noise and EMI. | |
| 7 | BOOT | P | Bootstrap pin for internal high-side driver circuitry. A 100-nF bootstrap capacitor is internally connected from this pin to SW within the module to provide the bootstrap voltage. | |
| 8 | VCC | P | Internal LDO output. Used as supply to internal control circuits. Do not connect to external loads. Can be used as logic supply for power-good flag. Connect a high-quality 1-µF capacitor from this pin to GND. | |
| 9 | FB |
A | Feedback input. For the adjustable
output, connect the mid-point of the feedback resistor divider to this pin. Connect
the upper resistor (RFBT) of the feedback divider to VOUT at the desired
point of regulation. Connect the lower resistor (RFBB) of the feedback
divider to GND. When connecting with feedback resistor divider, keep this FB trace
short and as small as possible to avoid noise coupling. See Section 8.5.2 for a feedback
resistor placement. |
|
| 10 | GND | G | Power ground terminal. Connect to system ground. Connect to CIN with short, wide traces. | |
| 11 | RT or MODE/SYNC | A | When the part is configured as the RT pin variant, the switching frequency in the part can be adjusted from 200 kHz to 2.2 MHz based on the resistor value connected between RT and GND.When the pin is trimmed as the MODE/SYNC variant, the part can operate in user-selectable PFM/PWM operation. In FPWM, the part can be synchronized to an external clock. Clock triggers on rising edge of applied external clock.Do not float this pin.. | |
| A = Analog, P = Power, G = Ground | ||||