JAJSBH1D July 2011 – October 2016
PRODUCTION DATA.
The bq76925 Host-controlled analog front end (AFE) is part of a complete pack monitoring, balancing, and protection system for 3-series to 6-series cell Lithium batteries. The bq76925 allows a Host controller to easily monitor individual cell voltages, pack current, and temperature. The Host may use this information to detect and act on a fault condition caused when one or more of these parameters exceed the limits of the application. In addition, the Host may use this information to determine end-of-charge, end-of-discharge, and other gas-gauging and state of health conditions.
The bq76925 device provides a regulated 3.3-V supply voltage on the V3P3 pin for operating the device’s internal logic and interface circuitry. This regulator may also be used to directly power an external microcontroller or other external circuitry up to a limit of 4-mA load current. In this configuration, the VCTL pin is tied directly to the BAT pin. For applications requiring more than 4 mA, an external-bypass transistor may be used to supply the load current. In this configuration, the VCTL pin is tied to the gate of the bypass FET. These two configurations are show in Figure 9.
For the configuration of Figure 9b), a high-gain bypass device should be used to ensure stability. A bipolar PNP or p-channel FET bypass device may be used. Contact TI for recommendations.
The LDO regulator may be overridden (that is, back-fed) by an external-supply voltage greater than the regulated voltage on V3P3. In this configuration, the bq76925 internal logic and interface circuitry operates from the external supply and the internal 3.3-V regulator supplys no load current.
The bq76925 device is designed to interface to a multi-channel analog-to-digital converter (ADC) located in an external Host controller, such as an MSP430 Microcontroller or equivalent. Three outputs provide voltage, current, and temperature information for measurement by the Host. In addition, the bq76925 device includes a low-drift calibrated 1.5 / 3 V reference that is output on a dedicated pin for use as the reference input to the ADC.
The gain and offset characteristics of the bq76925 device are measured during factory test and stored in non-volatile memory as correction factors. The Host reads these correction factors and applies them to the ADC conversion results in order to achieve high-measurement accuracy. In addition, the precise voltage reference of the bq76925 can be used to calibrate the gain and offset of the Host ADC.
The bq76925 device outputs a stable reference voltage for use by the Host ADC. A nominal voltage of 1.5 V or 3 V is selected through the REF_SEL bit in the CONFIG_2 register. The reference voltage is very stable across temperature, but the initial voltage may vary by ±4%. The variation from nominal is manifested as a gain error in the ADC conversion result. To correct for this error, offset and gain correction factors are determined at final test and stored in the non-volatile registers VREF_CAL and VREF_CAL_EXT. The Host reads the correction factors and applies them to the nominal reference voltage to arrive at the actual reference voltage as described under Cell Voltage Monitoring. After gain correction, the tolerance of the reference will be within ±0.1%.
All analog-to-digital converters have inherent gain and offset errors, which adversely affect measurement accuracy. Some microcontrollers may be characterized by the manufacturer and shipped with ADC gain and offset information stored on-chip. It is also possible for such characterization to be done by the end-user on loose devices prior to PCB assembly or as a part of the assembled PCB test.
For applications where such ADC characterization is not provided or is not practical, the bq76925 device provides a means for in-situ calibration of the Host ADC through setting of the VCOUT_SEL bits in the CELL_CTL register two scaled versions of the reference voltage, 0.5 × VREF and 0.85 × VREF, can be selected for output on the VCOUT pin for measurement by the Host ADC. Measuring both scaled voltages enables the Host to do a two-point calibration of the ADC and compensate for the ADC offset and gain in all subsequent ADC measurement results as shown in Figure 10.
Note that the calibration accuracy will be limited by the tolerance of the scaled reference-voltage output so that use of this method may not be effective. For these cases, TI recommends to use a higher-accuracy source for the two-point calibration shown in Figure 10.
The cell-voltage monitoring circuits include an input level-shifter, multiplexer (MUX), and scaling amplifier. The Host selects one VCn cell input for measurement by setting the VCOUT_SEL and CELL_SEL bits in the CELL_CTL register. The scaling factor is set by the REF_SEL bit in the CONFIG_2 register. The selected cell input is level shifted to VSS reference, scaled by a nominal gain GVCOUT = 0.3 (REF_SEL = 0) or 0.6 (REF_SEL = 1) and output on the VCOUT pin for measurement by the Host ADC.
Similar to the reference voltage, gain and offset correction factors are determined at final test for each individual cell input and stored in non-volatile registers VCn_CAL (n = 1-6) and VC_CAL_EXT_m (m = 1-2). These factors are read by the Host and applied to the ADC voltage-measurement results in order to obtain the specified accuracy.
The cell voltage offset and gain correction factors are stored as 5-bit signed integers in 2’s complement format. The most significant bits (VCn_OC_4, VCn_GC_4) are stored separately and must be concatenated with the least significant bits (VCn_OFFSET_CORR, VCn_GAIN_CORR).
The reference voltage offset and gain correction factors are stored respectively as a 6-bit and 5-bit signed integer in 2’s complement format. As with the cell voltage correction factors, the most significant bits (VREF_OC_5, VREF_OC_4, VREF_GC_4) are stored separately and must be concatenated with the least significant bits (VREF_OFFSET_CORR, VREF_GAIN_CORR).
The actual cell voltage (VCn) is calculated from the measured voltage (VCOUT) as shown in the following equations:
For cell voltages across (VC1 – VC0) that are less than approximately 2.64 V, extreme cell-voltage imbalances between (VC1 – VC0) and (VC2 – VC1) can lead to a loss of gain in the (VC2 – VC1) amplifier. The cell imbalance at which the loss of gain occurs is determined by Equation 3:
Assuming VC0 = VSS, it can be seen that when (VC1 – VC0) > 2.64 volts, the voltage across (VC2 – VC1) can range up to the limit of 4.4 V without any loss of gain. At the minimum value of (VC1 – VC0) = 1.4 V, an imbalance of more than 900 mV is tolerated before any loss of gain in the (VC2 – VC1) amplifier. For higher values of (VC1 – VC0), increasingly large imbalances are tolerated. For example, when (VC1 – VC0) = 2.0 V, an imbalance up to 1.33 V (that is, (VC2 – VC1) = 3.33 V) results in no degradation of amplifier performance.
Normally, cell imbalances greater than 900 mV will signal a faulty condition of the battery pack and its use should be discontinued. The loss of gain on the second cell input does not affect the ability of the system to detect this condition. The gain fall-off is gradual so that the measured imbalance will never be less than the critical imbalance set by Equation 3.
Therefore, if the measured (VC2 – VC1) is greater than (VC1 – VSS) / 0.6, a severe imbalance is detected and the pack should enter a fault state which prevents further use. In this severe cell imbalance condition comparisons of the measured (VC2 – VC1) to any overvoltage limits will be optimistic due to the reduced gain in the amplifier, further emphasizing the need to enter a fault state.
Voltage differences between BAT and the top cell potential come from two sources as shown in Figure 11: V3P3 regulator current that flows through the RBAT filter resistor, and the voltage drop in the series diode DBAT of the hold-up circuit. These effects cause BAT to be less than the top-cell voltage measured by the cell amplifier.
The top-cell amplifier (VC6 – VC5) is designed to measure an input voltage down to 1.4 V with a difference between the BAT and VC6 pin up to 1.2 V (that is, BAT can be 1.2 V lower than VC6). However, in applications with fewer than 6 cells, the upper-cell inputs are typically shorted to the top-cell input. For example, in a 5-cell application VC6 and VC5 would be shorted together and the (VC5 – VC4) amplifier would measure the top-cell voltage. The case is similar for 4-cell and 3-cell applications.
For these cases when using the (VC5 – VC4), (VC4 –VC3), or (VC3 – VC2) amplifier to measure the top cell, the difference between BAT and the top-cell amplifier must be less than 240 mV in order to measure cell voltages down to 1.4 V. Note that at higher-cell input voltages the top amplifier tolerates a greater difference. For example, in a 5-cell configuration (VC6 and VC5 tied together) the (VC5 – VC4) amplifier is able to measure down to a 1.7 V input with a 600-mV difference between VC5 and BAT.
Accordingly, in systems with fewer than 6 cells, it is important in system design to minimize RBAT and to use a Schottky type diode for DBAT with a low forward voltage. If it is not possible to reduce the drop at BAT to an acceptable level, then for 4-cell and 5-cell configurations, the (VC6 – VC5) amplifier may be used as the top cell amplifier as shown in Table 1, which allows up to a 1.2 V difference between BAT and the top cell.
Configuration | Cell 5 | Cell 4 | Cell 3 | Cell 2 | Cell 1 | Unused Cell Inputs |
---|---|---|---|---|---|---|
5-cell | VC6 – VC5 | VC4 – VC3 | VC3 – VC2 | VC2 – VC1 | VC1 – VC0 | Short VC5 to VC4 |
4-cell | VC6 – VC5 | VC3 – VC2 | VC2 – VC1 | VC1 – VC0 | Short VC5 to VC4 to VC3 |
Current is measured by converting current to voltage through a sense resistor connected between SENSEN and SENSEP. A positive voltage at SENSEP with respect to SENSEN indicates a discharge current is flowing, and a negative voltage indicates a charge current. The small voltage developed across the sense resistor is amplified by gain GVIOUT and output on the VIOUT pin for conversion by the Host ADC. The voltage on VIOUT is always positive and for zero current is set to 3/4 of the output range. The current sense amplifier is inverting; discharge current causes VIOUT to decrease and charge current causes VIOUT to increase. Therefore, the measurement range for discharge currents is 3 times the measurement range for charge currents.
The current-sense amplifier is preceded by a multiplexer that allows measurement of either the SENSEN or SENSEP input with respect to VSS. The Host selects the pin for measurement by writing the I_AMP_CAL bit in the CONFIG_1 register. The Host then calculates the voltage across the sense resistor by subtracting the measured voltage at SENSEN from the measured voltage at SENSEP. If the SENSEN and VSS connections are such that charge and discharge currents do not flow through the connection between them; that is, there is no voltage drop between SENSEN and VSS due to the current being measured, then the measurement of the SENSEN voltage can be regarded as a calibration step and stored by the Host for use as a pseudo-constant in the VSENSE calculation. The SENSEN voltage measurement would then only need updating when changing environmental conditions warrant.
The Host sets GVIOUT by writing the I_GAIN bit in the CONFIG_1 register. The available gains of 4 and 8 enable operation with a variety of sense-resistor values over a broad range of pack currents. The gain may be changed at any time allowing for dynamic range and resolution adjustment. The input and output ranges of the amplifier are determined by the value of the REF_SEL bit in the CONFIG_2 register. These values are shown in Table 2. Because the current amplifier is inverting, the Min column under Output Range corresponds to the Max column under Input Range. Likewise, the Max column under Output Range corresponds to the Min column under Input Range.
The actual current is calculated from the measured voltage (VIOUT) as follows. Note that VSENSE is positive when discharge current is flowing. In keeping with battery pack conventions, the sign of ISENSE is inverted so that discharge current is negative.
REF_SEL | I_GAIN | Gain | VIOUT (V) at ISENSE = 0 (typical) |
Input Range(1)
(mV) |
Output Range(3)
(V) |
ISENSE Range (A) at RSENSE = 1 mΩ |
ISENSE Resolution (mA)w/10-bit ADC(2) | ||
---|---|---|---|---|---|---|---|---|---|
Min | Max | Min | Max | ||||||
0 | 0 | 4 | 1.0 | –62.5 | 187.5 | 0.25 | 1.25 | –62.5 – 187.5 | 366 |
0 | 1 | 8 | 1.0 | –14 | 91 | 0.27 | 1.11 | –14 – 91 | 183 |
1 | 0 | 4 | 2.0 | –125 | 375 | 0.5 | 2.5 | –125 – 375 | 732 |
1 | 1 | 8 | 2.0 | –62.5 | 187.5 | 0.5 | 2.5 | –62.5 – 187.5 | 366 |
The bq76925 device also includes a comparator for monitoring the current-sense resistor and alerting the Host when the voltage across the sense resistor exceeds a selected threshold. The available thresholds range from 25 mV to 400 mV and are set by writing the I_THRESH bits in the CONFIG_1 register. Positive (discharge) or negative (charge) current may be monitored by setting the I_COMP_POL bit in the CONFIG_1 register. By the choice of sense resistor and threshold, a variety of trip points are possible to support a wide range of applications.
The comparator result is driven through the open-drain ALERT output to signal the host when the threshold is exceeded. This feature can be used to wake up the Host on connection of a load or to alert the Host to a potential fault condition. The ALERT pin state is also available by reading the ALERT bit in the STATUS register.
To enable temperature measurements by the Host, the bq76925 device provides the LDO regulator voltage on a separate output pin (VTB) for biasing an external thermistor network. In order to minimize power consumption, the Host may switch the VTB output on and off by writing to the VTB_EN bit in the POWER_CTL register. Note that if the LDO is back-fed by an external source, the VTB bias will be switched to the external source.
In a typical application, the thermistor network will consist of a resistor in series with an NTC thermistor, forming a resistor divider where the output is proportional to temperature. This output may be measured by the Host ADC to determine temperature.
The internal temperature (TINT) of the bq76925 device can be measured by setting VCOUT_SEL = ‘01’ and CELL_SEL = ‘110’ in the CELL_CTL register. In this configuration, a voltage proportional to temperature (VTEMP_INT) is output on the VCOUT pin. This voltage is related to the internal temperature as follows:
The bq76925 device integrates cell-balancing FETs that are individually controlled by the Host. The balancing method is resistive bleed balancing, where the balancing current is set by the external cell input resistors. The maximum allowed balancing current is 50 mA per cell.
The Host may activate one or more cell balancing FETs by writing the BAL_n bits in the BAL_CTL register. To allow the greatest flexibility, the Host has complete control over the balancing FETs. However, in order to avoid exceeding the maximum cell input voltage, the bq76925 will prevent two adjacent balancing FETs from being turned on simultaneously. If two adjacent bits in the balance control register are set to 1, neither balancing transistor will be turned on. The Host based balancing algorithm must also limit the power dissipation to the maximum ratings of the device.
In a normal system, closing a cell-balancing FET will cause 2 cell voltages to appear across one cell input. This fact can be utilized to detect a cell sense-line open condition, that is, a broken wire from the cell-sense point to the bq76925 VCn input. Table 3 shows how this can be accomplished. Note that the normal cell-voltage measurements may represent a saturated or full-scale reading. However, these will normally be distinguishable from the open-cell measurement.
Kelvin input to test | Method 1 | Method 2 | ||||||
---|---|---|---|---|---|---|---|---|
Turn On | Measure | Result | Turn On | Measure | Result | |||
Normal | Open | Normal | Open | |||||
VC0 | BAL_1 | CELL2 | CELL2 + 0.5 × CELL1 | CELL2 | ||||
VC1 | BAL_2 | CELL3 | CELL3 + 0.5 × CELL2 | CELL3 | ||||
VC2 | BAL_3 | CELL4 | CELL4 + 0.5 × CELL3 | CELL4 | BAL_2 | CELL1 | CELL1 + 0.5 × CELL2 | CELL1 |
VC3 | BAL_4 | CELL5 | CELL5 + 0.5 × CELL4 | CELL5 | BAL_3 | CELL2 | CELL2 + 0.5 × CELL3 | CELL2 |
VC4 | BAL_5 | CELL6 | CELL6 + 0.5 × CELL5 | CELL6 | BAL_4 | CELL3 | CELL3 + 0.5 × CELL4 | CELL3 |
VC5 | BAL_5 | CELL4 | CELL4 + 0.5 × CELL5 | CELL4 | ||||
VC6 | BAL_6 | CELL5 | CELL5 + 0.5 × CELL6 | CELL5 |
Note that the cell amplifier headroom limits discussed above apply to the open-cell detection method because by virtue of closing a switch between 2 cell inputs, internal to the device this appears as an extreme cell imbalance. Therefore, when testing for an open on CELL2 by closing the CELL1 balancing FET, the CELL2 measurement will be less than the expected normal result due to gain loss caused by the imbalance. However, the CELL2 measurement will still increase under this condition so that a difference between open (no change) and normal (measured voltage increases) can be detected.
When initially powering up the bq76925 device, the voltage on the BAT pin must exceed VPOR (4.7-V maximum) before the device will turn on. Following this, the device will remain operational as long as the voltage on BAT remains above VSHUT (3.6-V maximum). If the BAT voltage falls below VSHUT, the device will shut down. Recovery from shutdown occurs when BAT rises back above the VPOR threshold and is equivalent to a POR. The VPOR threshold following a shutdown depends on the minimum level reached by BAT after crossing below VSHUT. If BAT does not fall below approximately 1.4 V, a higher VPOR (7.5-V maximum) applies. This is illustrated in Figure 12.
Following a power on reset, all volatile registers assume their default state. Therefore, care must be taken that transients on the BAT pin during normal operation do not fall below VSHUT. To avoid this condition in systems subject to extreme transients or brown-outs, a hold-up circuit such as the one shown in the functional diagram is recommended. When using a hold-up circuit, care must be taken to observe the BAT to VC6 maximum ratings.
Individual device functions such as cell translator, current amplifier, reference, and current comparator can be enabled and disabled under Host control by writing to the POWER_CTL register. The STANDBY feature can be used to save power by disabling functions that are unused. In the minimum power standby mode, all device functions can be turned off leaving only the 3.3-V regulator active.
In addition to STANDBY, there is also a SLEEP mode. In SLEEP mode the Host orders the bq76925 device to shutdown all internal circuitry and all functions including the LDO regulator. The device consumes a minimal amount of current (< 1.5 μA) in SLEEP mode due only to leakage and powering of the wake-up detection circuitry.
SLEEP mode is entered by writing a ‘1’ to the SLEEP bit in the POWER_CTL register. Wake-up is achieved by pulling up the ALERT pin; however, the wake-up circuitry is not armed until the voltage at V3P3 drops to approximately 0 V. To facilitate the discharge of V3P3, an internal 3-kΩ pulldown resistor is connected from V3P3 to VSS during the time that sleep mode is active. Once V3P3 is discharged, the bq76925 may be awakened by pulling the ALERT pin above VWAKE (2-V maximum).
The SLEEP_DIS bit in the POWER_CTL register acts as an override to the SLEEP function. When SLEEP_DIS is set to ‘1’, writing the SLEEP bit has no effect (that is, SLEEP mode cannot be entered). If SLEEP_DIS is set after SLEEP mode has been entered, the device will immediately exit SLEEP mode. This scenario can arise if SLEEP_DIS is set after SLEEP is set, but before V3P3 has discharged below a valid operating voltage. This scenario can also occur if the V3P3 pin is held up by external circuitry and not allowed to fully discharge.
If the overcurrent alert function is not used, the ALERT pin can function as a dedicated wake-up pin. Otherwise, the ALERT pin will normally be pulled up to the LDO voltage, so care must be taken in the system design so that the wake-up signal does not interfere with proper operation of the regulator.
The Host communicates with the AFE through an I2C interface. A CRC byte may optionally be used to ensure robust operation. The CRC is calculated over all bytes in the message according to the polynomial x8 + x2 + x + 1.
In order to reduce communications overhead, the addressing scheme for the I2C interface combines the slave device address and device register addresses into a single 7-bit address as shown below.
ADDRESS[6:0] = (I2C_GROUP_ADDR[3:0] << 3) + REG_ADDR[4:0]
The I2C_GROUP_ADDR is a 4-bit value stored in the EEPROM. REG_ADDR is the 5-bit register address being accessed, and can range from 0x00 – 0x1F. The factory programmed value of the group address is ‘0100’. Contact TI if an alternative group address is required.
For the default I2C_GROUP_ADDR, the combined address can be formed as shown in Table 4.
ADDRESS[6:0] | ||
---|---|---|
6 | 5 | 4:0 |
0 | 1 | Register address |
The Host writes to the registers of the bq76925 device as shown in Figure 13. The bq76925 acknowledges each received byte by pulling the SDA line low during the acknowledge period.
The Host may optionally send a CRC after the Data byte as shown. The CRC for write commands is enabled by writing the CRC_EN bit in the CONFIG_2 register. If the CRC is not used, then the Host generates the Stop condition immediately after the bq76925 acknowledges receipt of the Data byte.
When the CRC is disabled, the bq76925 device will act on the command on the first rising edge of SCL following the ACK of the Data byte. This occurs as part of the normal bus setup prior to a Stop. If a CRC byte is sent while the CRC is disabled, the first rising edge of the SCL following the ACK will be the clocking of the first bit of the CRC. The bq76925 device does not distinguish these two cases. In both cases, the command will complete normally, and in the latter case the CRC will be ignored.
The Host reads from the registers of the bq76925 device as shown in Figure 14. This protocol is similar to the write protocol, except that the slave now drives data back to the Host. The bq76925 device acknowledges each received byte by pulling the SDA line low during the acknowledge period. When the bq76925 device sends data back to the Host, the Host drives the acknowledge.
The Host may optionally request a CRC byte following the Data byte as shown. The CRC for read commands is always enabled, but not required. If the CRC is not used, then the Host simply NACK’s the Data byte and then generates the Stop condition.
Address | Name | Access | D7 | D6 | D5 | D4 | D3 | D2 | D1 | D0 |
---|---|---|---|---|---|---|---|---|---|---|
0x00 | STATUS | R/W | ALERT | CRC_ERR | POR | |||||
0x01 | CELL_CTL | R/W | VCOUT_SEL | CELL_SEL | ||||||
0x02 | BAL_CTL | R/W | BAL_6 | BAL_5 | BAL_4 | BAL_3 | BAL_2 | BAL_1 | ||
0x03 | CONFIG_1 | R/W | I_THRESH | I_COMP_POL | I_AMP_CAL | I_GAIN | ||||
0x04 | CONFIG_2 | R/W | CRC_EN | REF_SEL | ||||||
0x05 | POWER_CTL | R/W | SLEEP | SLEEP_DIS | I_COMP_EN | I_AMP_EN | VC_AMP_EN | VTB_EN | REF_EN | |
0x06 | Reserved | R/W | ||||||||
0x07 | CHIP_ID | RO | CHIP_ID | |||||||
0x08 – 0x0F | Reserved | R/W | ||||||||
0x10 | VREF_CAL | EEPROM | VREF_OFFSET_CORR | VREF_GAIN_CORR | ||||||
0x11 | VC1_CAL | EEPROM | VC1_OFFSET_CORR | VC1_GAIN_CORR | ||||||
0x12 | VC2_CAL | EEPROM | VC2_OFFSET_CORR | VC2_GAIN_CORR | ||||||
0x13 | VC3_CAL | EEPROM | VC3_OFFSET_CORR | VC3_GAIN_CORR | ||||||
0x14 | VC4_CAL | EEPROM | VC4_OFFSET_CORR | VC4_GAIN_CORR | ||||||
0x15 | VC5_CAL | EEPROM | VC5_OFFSET_CORR | VC5_GAIN_CORR | ||||||
0x16 | VC6_CAL | EEPROM | VC6_OFFSET_CORR | VC6_GAIN_CORR | ||||||
0x17 | VC_CAL_EXT_1 | EEPROM | VC1_OC_4 | VC1_GC_4 | VC2_OC_4 | VC2_GC_4 | ||||
0x18 | VC_CAL_EXT_2 | EEPROM | VC3_OC_4 | VC3_GC_4 | VC4_OC_4 | VC4_GC_4 | VC5_OC_4 | VC5_GC_4 | VC6_OC_4 | VC6_GC_4 |
0x10 – 0x1A | Reserved | EEPROM | ||||||||
0x1B | VREF_CAL_EXT | EEPROM | 1 | VREF_OC_5 | VREF_OC_4 | VREF_GC_4 | ||||
0x1C – 0x1F | Reserved | EEPROM |
Address | Name | Type | D7 | D6 | D5 | D4 | D3 | D2 | D1 | D0 |
---|---|---|---|---|---|---|---|---|---|---|
0x00 | STATUS | R/W | ALERT | CRC_ERR | POR | |||||
Defaults: | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 |
ALERT: Over-current alert. Reflects state of the over-current comparator. ‘1’ = over-current.
CRC_ERR: CRC error status. Updated on every I2C write packet when CRC_EN = ‘1’. ‘1’ = CRC error.
POR: Power on reset flag. Set on each power-up and wake-up from sleep. May be cleared by writing with ‘0’.
Address | Name | Type | D7(1) | D6 | D5 | D4 | D3 | D2 | D1 | D0 |
---|---|---|---|---|---|---|---|---|---|---|
0x01 | CELL_CTL | R/W | VCOUT_SEL | CELL_SEL | ||||||
Defaults: | 0 | 0 | 0 | 0 | 0 |
VCOUT_SEL: VCOUT MUX select. Selects the VCOUT pin function as follows.
VCOUT_SEL | VCOUT |
---|---|
0 0 | VSS |
0 1 | VCn (n determined by CELL_SEL) |
1 0 | VREF × 0.5 |
1 1 | VREF × 0.85 |
CELL_SEL: Cell select. Selects the VCn input for output on VCOUT when VCOUT_SEL = ‘01’.
VCOUT_SEL | CELL_SEL | VCOUT |
---|---|---|
0 1 | 0 0 0 | VC1 |
0 1 | 0 0 1 | VC2 |
0 1 | 0 1 0 | VC3 |
0 1 | 0 1 1 | VC4 |
0 1 | 1 0 0 | VC5 |
0 1 | 1 0 1 | VC6 |
0 1 | 1 1 0 | VTEMP,INT |
0 1 | 1 1 1 | Hi-Z |
Address | Name | Type | D7 | D6 | D5 | D4 | D3 | D2 | D1 | D0 |
---|---|---|---|---|---|---|---|---|---|---|
0x02 | BAL_CTL | R/W | BAL_6 | BAL_5 | BAL_4 | BAL_3 | BAL_2 | BAL_1 | ||
Defaults: | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
BAL_n: Balance control for cell n. When set, turns on balancing transistor for cell n. Setting of two adjacent balance controls is not permitted. If two adjacent balance controls are set, neither cell balancing transistor will be turned on. However, the BAL_n bits will retain their values.
Address | Name | Type | D7 | D6 | D5 | D4 | D3 | D2 | D1 | D0 |
---|---|---|---|---|---|---|---|---|---|---|
0x03 | CONFIG_1 | R/W | I_THRESH | I_COMP_POL | I_AMP_CAL | I_GAIN | ||||
Defaults: | 0 | 0 | 0 | 0 | 0 |
I_THRESH: Current comparator threshold. Sets the threshold of the current comparator as follows:
I_THRESH | Comparator Threshold |
---|---|
0x0 | 25 mV |
0x1 | 50 mV |
0x2 | 75 mV |
0x3 | 100 mV |
0x4 | 125 mV |
0x5 | 150 mV |
0x6 | 175 mV |
0x7 | 200 mV |
0x8 | 225 mV |
0x9 | 250 mV |
0xA | 275 mV |
0xB | 300 mV |
0xC | 325 mV |
0xD | 350 mV |
0xE | 375 mV |
0xF | 400 mV |
I_COMP_POL: Current comparator polarity select. When ‘0’, trips on discharge current (SENSEP > SENSEN). When ‘1’, trips on charge current (SENSEP < SENSEN).
I_AMP_CAL: Current amplifier calibration. When ‘0’, current amplifier reports SENSEN with respect to VSS. When ‘1’, current amplifier reports SENSEP with respect to VSS. This bit can be used for offset cancellation as described under OPERATIONAL OVERVIEW.
I_GAIN: Current amplifier gain. Sets the nominal gain of the current amplifier as follows.
I_GAIN | Current amp gain |
---|---|
0 | 4 |
1 | 8 |
Address | Name | Type | D7 | D6 | D5 | D4 | D3 | D2 | D1 | D0 |
---|---|---|---|---|---|---|---|---|---|---|
0x04 | CONFIG_2 | R/W | CRC_EN | REF_SEL | ||||||
Defaults: | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
CRC_EN: CRC enable. Enables CRC comparison on write. When ‘1’, CRC is enabled. CRC on read is always enabled but is optional for Host.
REF_SEL: Reference voltage selection. Sets reference voltage output on VREF pin, cell-voltage amplifier gain and VIOUT output range.
REF_SEL | VREF (V) | VCOUT Gain | VIOUT Output Range (V) |
---|---|---|---|
0 | 1.5 | 0.3 | 0.25 – 1.25 |
1 | 3.0 | 0.6 | 0.5 – 2.5 |
Address | Name | Type | D7 | D6 | D5 | D4 | D3 | D2 | D1 | D0 |
---|---|---|---|---|---|---|---|---|---|---|
0x05 | POWER_CTL | R/W | SLEEP | SLEEP_DIS | I_COMP_EN | I_AMP_EN | VC_AMP_EN | VTB_EN | REF_EN | |
Defaults: | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
SLEEP: Sleep control. Set to ‘1’ to put device to sleep
SLEEP_DIS: Sleep mode disable. When ‘1’, disables the sleep mode.
I_COMP_EN: Current comparator enable. When ‘1’, comparator is enabled. Disable to save power.
I_AMP_EN: Current amplifier enable. When ‘1’, current amplifier is enabled. Disable to save power.
VC_AMP_EN: Cell amplifier enable. When ‘1’, cell amplifier is enabled. Disable to save power.
VTB_EN: Thermistor bias enable. When ‘1’, the VTB pin is internally switched to the V3P3 voltage.
REF_EN: Voltage reference enable. When ‘1’, the 1.5 / 3.0 V reference is enabled. Disable to save power
Address | Name | Type | D7 | D6 | D5 | D4 | D3 | D2 | D1 | D0 |
---|---|---|---|---|---|---|---|---|---|---|
0x07 | CHIP_ID | RO | CHIP_ID | |||||||
Defaults: | 0x10 |
CHIP_ID: Silicon version identifier.
Address | Name | Type | D7 | D6 | D5 | D4 | D3 | D2 | D1 | D0 |
---|---|---|---|---|---|---|---|---|---|---|
0x10 | VREF_CAL | EEPROM | VREF_OFFSET_CORR | VREF_GAIN_CORR |
VREF_OFFSET_CORR: Lower 4 bits of offset-correction factor for reference output. The complete offset-correction factor is obtained by concatenating this value with the the two most significant bits VREF_OC_5 and VREF_OC_4, which are stored in the VREF_CAL_EXT register. The final value is a 6-bit signed 2’s complement number in the range –32 to +31 with a value of 1 mV per LSB. See description of usage in Detailed Description.
VREF_GAIN_CORR: Lower 4 bits of gain correction factor for reference output. The complete gain correction factor is obtained by concatenating this value with the most significant bit VREF_GC_4, which is stored in the VREF_CAL_EXT register. The final value is a 5-bit signed 2’s complement number in the range –16 to +15 with a value of 0.1% per lsb. See description of usage in Detailed Description.
Address | Name | Type | D7 | D6 | D5 | D4 | D3 | D2 | D1 | D0 |
---|---|---|---|---|---|---|---|---|---|---|
0x11 | VC1_CAL | EEPROM | VC1_OFFSET_CORR | VC1_GAIN_CORR |
VC1_OFFSET_CORR: Lower 4 bits of offset correction factor for cell 1 translation. The complete offset correction factor is obtained by concatenating this value with the most significant bit VC1_OC_4, which is stored in the VC_CAL_EXT_1 register. The final value is a 5-bit signed 2’s complement number in the range -16 to +15 with a value of 1 mV per lsb. See description of usage in Detailed Description.
VC1_GAIN_CORR: Lower 4 bits of gain correction factor for cell 1 translation. The complete gain correction factor is obtained by concatenating this value with the most significant bit VC1_GC_4, which is stored in the VC_CAL_EXT_1 register. The final value is a 5-bit signed 2’s complement number in the range -16 to +15 with a value of 0.1% per lsb. See description of usage in Detailed Description.
Address | Name | Type | D7 | D6 | D5 | D4 | D3 | D2 | D1 | D0 |
---|---|---|---|---|---|---|---|---|---|---|
0x12 | VC2_CAL | EEPROM | VC2_OFFSET_CORR | VC2_GAIN_CORR |
VC2_OFFSET_CORR: Lower 4 bits of offset correction factor for cell 2 translation. The complete offset correction factor is obtained by concatenating this value with the most significant bit VC2_OC_4, which is stored in the VC_CAL_EXT_1 register. The final value is a 5-bit signed 2’s complement number in the range –16 to +15 with a value of 1 mV per LSB. See description of usage in See description of usage in Detailed Description.
VC2_GAIN_CORR: Lower 4 bits of gain correction factor for cell 2 translation. The complete gain correction factor is obtained by concatenating this value with the most significant bit VC2_GC_4, which is stored in the VC_CAL_EXT_1 register. The final value is a 5-bit signed 2’s complement number in the range –16 to +15 with a value of 0.1% per LSB. See description of usage in Detailed Description.
Address | Name | Type | D7 | D6 | D5 | D4 | D3 | D2 | D1 | D0 |
---|---|---|---|---|---|---|---|---|---|---|
0x13 | VC3_CAL | EEPROM | VC3_OFFSET_CORR | VC3_GAIN_CORR |
VC3_OFFSET_CORR: Lower 4 bits of offset correction factor for cell 3 translation. The complete offset correction factor is obtained by concatenating this value with the most significant bit VC3_OC_4, which is stored in the VC_CAL_EXT_2 register. The final value is a 5-bit signed 2’s complement number in the range –16 to +15 with a value of 1 mV per lsb. See description of usage in Detailed Description.
VC3_GAIN_CORR: Lower 4 bits of gain correction factor for cell 3 translation. The complete gain correction factor is obtained by concatenating this value with the most significant bit VC3_GC_4, which is stored in the VC_CAL_EXT_2 register. The final value is a 5-bit signed 2’s complement number in the range –16 to +15 with a value of 0.1% per lsb. See description of usage in Detailed Description.
Address | Name | Type | D7 | D6 | D5 | D4 | D3 | D2 | D1 | D0 |
---|---|---|---|---|---|---|---|---|---|---|
0x14 | VC4_CAL | EEPROM | VC4_OFFSET_CORR | VC4_GAIN_CORR |
VC4_OFFSET_CORR: Lower 4 bits of offset correction factor for cell 4 translation. The complete offset correction factor is obtained by concatenating this value with the most significant bit VC4_OC_4, which is stored in the VC_CAL_EXT_2 register. The final value is a 5-bit signed 2’s complement number in the range –16 to +15 with a value of 1 mV per lsb. See description of usage in Detailed Description.
VC4_GAIN_CORR: Lower 4 bits of gain correction factor for cell 4 translation. The complete gain correction factor is obtained by concatenating this value with the most significant bit VC4_GC_4, which is stored in the VC_CAL_EXT_2 register. The final value is a 5-bit signed 2’s complement number in the range –16 to +15 with a value of 0.1% per lsb. See description of usage in Detailed Description.
Address | Name | Type | D7 | D6 | D5 | D4 | D3 | D2 | D1 | D0 |
---|---|---|---|---|---|---|---|---|---|---|
0x15 | VC5_CAL | EEPROM | VC5_OFFSET_CORR | VC5_GAIN_CORR |
VC5_OFFSET_CORR: Lower 4 bits of offset correction factor for cell 5 translation. The complete offset correction factor is obtained by concatenating this value with the most significant bit VC5_OC_4, which is stored in the VC_CAL_EXT_2 register. The final value is a 5-bit signed 2’s complement number in the range –16 to +15 with a value of 1 mV per LSB. See description of usage in Detailed Description.
VC5_GAIN_CORR: Lower 4 bits of gain correction factor for cell 5 translation. The complete gain correction factor is obtained by concatenating this value with the most significant bit VC5_GC_4, which is stored in the VC_CAL_EXT_2 register. The final value is a 5-bit signed 2’s complement number in the range –16 to +15 with a value of 0.1% per LSB. See description of usage in Detailed Description.
Address | Name | Type | D7 | D6 | D5 | D4 | D3 | D2 | D1 | D0 |
---|---|---|---|---|---|---|---|---|---|---|
0x16 | VC6_CAL | EEPROM | VC6_OFFSET_CORR | VC6_GAIN_CORR |
VC6_OFFSET_CORR: Lower 4 bits of offset correction factor for cell 6 translation. The complete offset correction factor is obtained by concatenating this value with the most significant bit VC6_OC_4, which is stored in the VC_CAL_EXT_2 register. The final value is a 5-bit signed 2’s complement number in the range –16 to +15 with a value of 1 mV per LSB. See description of usage in Detailed Description.
VC6_GAIN_CORR: Lower 4 bits of gain correction factor for cell 6 translation. The complete gain correction factor is obtained by concatenating this value with the most significant bit VC6_GC_4, which is stored in the VC_CAL_EXT_2 register. The final value is a 5-bit signed 2’s complement number in the range –16 to +15 with a value of 0.1% per LSB. See description of usage in Detailed Description.
Address | Name | Type | D7 | D6 | D5 | D4 | D3 | D2 | D1 | D0 |
---|---|---|---|---|---|---|---|---|---|---|
0x17 | VC_CAL_EXT_1 | EEPROM | VC1_OC_4 | VC1_GC_4 | VC2_OC_4 | VC2_GC_4 |
VC1_OC_4: Most significant bit of offset correction factor for cell 1 translation. See Table 18 register description for details.
VC1_GC_4: Most significant bit of gain correction factor for cell 1 translation. See Table 18 register description for details.
VC2_OC_4: Most significant bit of offset correction factor for cell 2 translation. See Table 19 register description for details.
VC2_GC_4: Most significant bit of gain correction factor for cell 2 translation. See Table 19 register description for details.
Address | Name | Type | D7 | D6 | D5 | D4 | D3 | D2 | D1 | D0 |
---|---|---|---|---|---|---|---|---|---|---|
0x18 | VC_CAL_EXT_2 | EEPROM | VC3_OC_4 | VC3_GC_4 | VC4_OC_4 | VC4_GC_4 | VC5_OC_4 | VC5_GC_4 | VC6_OC_4 | VC6_GC4 |
VC3_OC_4: Most significant bit of offset correction factor for cell 3 translation. See Table 20 register description for details.
VC3_GC_4: Most significant bit of gain correction factor for cell 3 translation. See Table 20 register description for details.
VC4_OC_4: Most significant bit of offset correction factor for cell 4 translation. See Table 21 register description for details.
VC4_GC_4: Most significant bit of gain correction factor for cell 4 translation. See Table 21 register description for details.
VC5_OC_4: Most significant bit of offset correction factor for cell 5 translation. See Table 22 register description for details.
VC5_GC_4: Most significant bit of gain correction factor for cell 5 translation. See Table 22 register description for details.
VC6_OC_4: Most significant bit of offset correction factor for cell 6 translation. See Table 23 register description for details.
VC6_GC_4: Most significant bit of gain correction factor for cell 6 translation. See Table 23 register description for details.
Address | Name | Type | D7 | D6 | D5 | D4 | D3 | D2 | D1 | D0 |
---|---|---|---|---|---|---|---|---|---|---|
0x1B | VREF_CAL_EXT | EEPROM | 1 | VREF_OC_5 | VCREF_OC_4 | VREF_GC4 |
VREF_OC_5: Most significant bit of offset correction factor for reference output. See Table 17 register description for details.
VREF_OC_4: Next most significant bit of offset correction factor for reference output. See Table 17 register description for details.
VREF_GC_4: Most significant bit of gain correction factor for reference output. See Table 17 register description for details.