JAJSFR7F June 2016 – May 2019 DRA710 , DRA714 , DRA716 , DRA718
PRODUCTION DATA.
デバイスごとのパッケージ図は、PDF版データシートをご参照ください。
NOTE
For more information, see the Initialization (ROM Code) section of the device TRM.
| SIGNAL NAME | DESCRIPTION | TYPE | BALL |
|---|---|---|---|
| sysboot0 | Boot Mode Configuration 0. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | F1 |
| sysboot1 | Boot Mode Configuration 1. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | E2 |
| sysboot2 | Boot Mode Configuration 2. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | E1 |
| sysboot3 | Boot Mode Configuration 3. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | C1 |
| sysboot4 | Boot Mode Configuration 4. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | D1 |
| sysboot5 | Boot Mode Configuration 5. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | D2 |
| sysboot6 | Boot Mode Configuration 6. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | B1 |
| sysboot7 | Boot Mode Configuration 7. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | B2 |
| sysboot8 | Boot Mode Configuration 8. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | C2 |
| sysboot9 | Boot Mode Configuration 9. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | D3 |
| sysboot10 | Boot Mode Configuration 10. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | A2 |
| sysboot11 | Boot Mode Configuration 11. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | B3 |
| sysboot12 | Boot Mode Configuration 12. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | C3 |
| sysboot13 | Boot Mode Configuration 13. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | C4 |
| sysboot14 | Boot Mode Configuration 14. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | A3 |
| sysboot15 | Boot Mode Configuration 15. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | B4 |