JAJSSJ5 December 2023 DRV8234
PRODUCTION DATA
In case 1, Equation 5 can be used. Choose the value of KMC_SCALE such that KMC is within the range of 0 to 255 with highest bit resolution. As an example, if KV= 0.01 and number of ripples per revolution, NR=10, KV/NR = 10-3. The following table lists the available options:
Bit | KMC_SCALE value | KV/NRx KMC_SCALE (Actual Value) | Rounded Value (KMC) | Comment |
---|---|---|---|---|
00b | 24 x 28 | 6.144 | 6 | Avoid selecting, since low bit precision. |
01b | 24 x 29 | 12.288 | 12 | Avoid selecting, since low bit precision. |
10b | 24 x 212 | 98.304 | 98 | Avoid selecting, since low bit precision. |
11b | 24 x 213 | 196.608 | 197 | Can select this value as this has the highest bit precision. |