JAJSH39A March 2019 – June 2019 LM66100
PRODUCTION DATA.
This circuit ties the CE of each device to the opposite power source. In this configuration, the highest supply will always be selected using a make-before-break logic. This prevents any reverse current flow between the supplies and avoids the need of a dedicated reverse current blocking comparator. For ORing applications that need RPP, it is recommended to use a series resistor (RCE) to limit the current into the CE pin during a negative voltage event.