JAJSR71 January 2024 LMR43606-Q1
PRODUCTION DATA
The LMR43606-Q1 is designed to have very low input supply current when regulating light loads. This design is achieved by powering much of the internal circuitry from the output. The VOUT/FB pin in the fixed-output voltage variants is the input to the LDO that powers the majority of the control circuits. By connecting the VOUT/FB input pin to the output node of the regulator, a small amount of current is drawn from the output. This current is reduced at the input by the ratio of VOUT / VIN as described in Equation 3.
where