To begin the design process, determine
the following:
- Input voltage range:
- Use the supply
voltage of the device that is driving the SN74LXCH1T45 device to
determine the input voltage range. The value must exceed the
high-level input voltage (VIH) of the input port for a
valid logic-high. The value must be less than the low-level input
voltage (VIL) of the input port for a valid logic
low.
- Output voltage range:
- Use the device's
supply voltage that the SN74LXCH1T45 device is driving to determine
the output voltage range.