JAJSIR1B March 2020 – December 2020 TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1
PRODUCTION DATA
The CAN module uses the IP known as DCAN. This document uses the names CAN and DCAN interchangeably to reference this peripheral.
The CAN module implements the following features:
For a CAN bit clock of 100 MHz, the smallest bit rate possible is 3.90625 kbps.
The accuracy of the on-chip zero-pin oscillator is in Section 7.11.3.5.1. Depending on parameters such as the CAN bit timing settings, bit rate, bus length, and propagation delay, the accuracy of this oscillator may not meet the requirements of the CAN protocol. In this situation, an external clock source must be used.
Figure 7-52 shows the CAN block diagram.