JAJSKO9A March 2020 – March 2021 TMUX4157N
PRODUCTION DATA
The TON (VSS) time is defined as the time taken by the output of the device to rise to 90% after the supply has risen past the supply threshold. The 90% measurement is used to provide the timing of the device turning on in the system. Figure 7-7 shows the setup used to measure turn on time, denoted by the symbol TON (VSS).