JAJSDD3B June 2017 – January 2019 TPS53681
PRODUCTION DATA.
Overcurrent thresholds are configured using the IOUT_OC_FAULT_LIMIT. When the overcurrent fault threshold is reached, the converter will respond according to the settings in IOUT_OC_FAULT_RESPONSE. The IOUT_OC_WARN_LIMIT may also be used to configure an information-only overcurrent warning, which triggers prior to an overcurrent fault. Note, that the MFR_SPECIFIC_00 command, not listed below, also contains settings for per-phase overcurrent limits. Refer to the device Technical Reference Manual for more information.