JAJSEF3B january 2018 – june 2023 TPS61280D , TPS61280E , TPS61281D
PRODUCTION DATA
In order to maintain a certain minimum output voltage under heavy load transients, the output voltage set point can be dynamically increased by asserting the VSEL input. The functionality also helps to mitigate undershoot during severe line transients, while minimizing the output voltage during more benign operating conditions to save power.
The output voltage ramps up (floor to roof transition) at pre-defined rate defined by the average input current limit setting. The required time to ramp down the voltage (roof to floor transition) largely depends on the amount of capacitance present at the converter's output as well as on the load current. Table 9-1 shows the ramp rate control when transitioning to a lower voltage.
Mode Associated with Floor Voltage | Output Voltage Ramp Rate |
---|---|
Forced PWM | Output capacitance is being discharged at a rate of approx. 50mA (or higher) constant current in addition to the load current drawn |
PFM | Output capacitance is being discharged (solely) by the load current drawn |