JAJS204T December 2005 – April 2025 TPS74401
PRODUCTION DATA
Figure 7-12 shows a typical application of the TPS74401 using an auxiliary bias rail. The auxiliary bias rail allows for the designer to specify the system to have a low VDO. The bias rail supplies the error amplifier with a higher supply voltage, increasing the voltage that can be applied to the gate of the pass device.
VBIAS must be at least VOUT + 1.62V.
Figure 7-12 Typical
Application of the TPS74401 Using an Auxiliary Bias Rail