JAJSGA2G September 2018 – June 2024 TPS2663
PRODUCTION DATA
Figure 5-1 TPS26630, TPS26631 RGE Package;24-Pin VQFN(Top View)
Figure 5-3 TPS26632, TPS26633, TPS26635, TPS26637 RGE
Package;24-Pin VQFN(Top View)
Figure 5-2 TPS26631 PWP Package,20-Pin HTSSOP(Top View)
Figure 5-4 TPS26633, TPS26636, TPS26637 PWP
Package;20-Pin HTSSOP(Top View)| PIN | TYPE(1) | DESCRIPTION | ||
|---|---|---|---|---|
| NAME | VQFN | HTSSOP | ||
| IN | 1 | 1 | P | Power input. Connects to the DRAIN of the internal FET. |
| 2 | 2 | |||
| — | 3 | |||
| B_GATE | 3 | 4 | O | Blocking FET gate driver output. Connect B_GATE to GATE of the external NFET. If external FET is not used then leave B_GATE pin floating. See the Input Reverse Polarity Protection (B_GATE, DRV) section. |
| DRV | 4 | 5 | O | Blocking FET fast pulldown switch drive. Connect DRV to the GATE of external pulldown switch. Leave this pin floating if external N-FET is not used. |
| IN_SYS | 5 | 6 | P | Power input and supply voltage of the device. When an external Blocking FET is used then connect IN_SYS to source of the FET. Short IN_SYS to IN in case blocking FET is not used. |
| UVLO | 6 | 7 | I | Input for setting the programmable undervoltage lockout threshold. An undervoltage event turns off the internal FET and asserts FLT to indicate the power-failure. Connect UVLO pin to GND pin to select the internal default threshold. |
| OVP | 7 | 8 | I | Input for setting the programmable overvoltage protection threshold (For TPS26630 and TPS26631 Only). An overvoltage event turns off the internal FET and asserts FLT to indicate the overvoltage fault. Connect OVP pin to GND pin externally to select the internal default threshold. |
| PLIM | 7 | 8 | I | Input for setting the programmable output power limiting threshold (For TPS26632, TPS26633, TPS26635,TPS26636 and TPS26637 Only). Connect a resistor across PLIM to GND to set the output power limit. Connect PLIM to GND if PLIM feature is not used. See the Output Power Limiting, PLIM (TPS26632, TPS26633, TPS26635 and TPS26636 Only) section. |
| GND | 8 | 9 | — | Connect GND to system ground. |
| dVdT | 9 | 10 | I/O | A capacitor from this pin to GND sets output voltage slew rate. See the Hot Plug-In and InRush Current Control section. |
| ILIM | 10 | 11 | I/O | A resistor from this pin to GND sets the overload and short-circuit current limit. See the Overload and Short-Circuit Protection section. |
| MODE | 11 | 12 | I | Mode selection pin for overload fault response. See the Device Functional Modes section. |
| SHDN | 12 | 13 | I | Shutdown pin. Pulling SHDN low makes the device to enter into low power shutdown mode. Cycling SHDN pin voltage resets the device that has latched off due to a fault condition. |
| IMON | 13 | 14 | O | Analog current monitor output. This pin sources a scaled down ratio of current through the internal FET. A resistor from this pin to GND converts current to proportional voltage. If unused, leave this pin floating. |
| FLT | 14 | 15 | O | Fault event indicator. This pin is an open drain output. If unused, leave floating or connect to GND. |
| PGTH | 15 | 16 | I | PGOOD comparator input. |
| PGOOD | 16 | 17 | O | Active High. A high indicates PGTH has crossed the V(PGTHR) threshold and the internal FET is enhanced. PGOOD goes low when V(PGTH) hits V(PGTHF) threshold. If PGOOD is unused then connect to GND or leave it floating. |
| OUT | 17 | 18 | P | Power output of the device. |
| 18 | 19 | |||
| — | 20 | |||
| N. C | 19 | — | — | No connect. |
| 20 | ||||
| 21 | ||||
| 22 | ||||
| 23 | ||||
| 24 | ||||
| PowerPAD™ integrated circuit package |
— | — | — | Connect PowerPAD integrated circuit package to GND plane for heat sinking. Do not use PowerPAD integrated circuit package as the only electrical connection to GND. |